Skip to main content
aberracasa
Associate
Jun 7, 2004 1:02 PM UTC
Question

SVF file format

Posted on June 07, 2004 at 15:02

SVF file format

This topic has been closed for replies.

1 reply

aberracasa
Associate
May 17, 2011 10:01 AM UTC
Posted on May 17, 2011 at 12:01

Hello,

I need to program a UPSD3234BV part in system via the JTAG port. As with other ISP devices, I generated a SVF file from the OBJ. I have the following questions:

1. While I understand the functionality of TERR and TSTAT I cannot see how the 2 SVF files (4-pin vs 6-pin) are to be used differently.

2. The SVF files are HUGE. I noticed that the programming is done in 11-bit chunks. Is there a way to create a smaller SVF file, a binary SVF file? I am trying to fit it into the system controller's FLASH.

Thank you,

Andre