Skip to main content
Associate III
September 1, 2025
Solved

STWD100NY Connection

I use STWD100NY Watchdog IC and for now, i can not achieve what i want. The problem is about to get output from the WDO pin. I did not connect the WDO to the MCU but i connect it to drive a relay. I set up my timer to 4 seconds. Even if it exceeds the twd time, i can not get the signal from WDO pin. I attach my drawings below and needs your help. My Vcc is 5V( most setups use 3.3v but i think that i can choose it 5V according to datasheet ). R25 and R26 resistors are optional.watchdog IC.png

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
September 1, 2025

If you control /EN with a voltage divider of 1k+1k, the STWD100 will never work because this results in a voltage of VCC/2. However, as shown in table 4 mentioned above, /EN requires a voltage of max. 30% VCC to enable the STWD100. This means that as long as /EN is not activated, WDO cannot be active either.

Incidentally, WDO is an open drain, which is why you have provided R134 as a pull-up. However, this also means that R40 is pointless and can be replaced by a short circuit.

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

17 replies

Peter BENSCH
ST Technical Moderator
September 1, 2025

Er... you want to drive a relay directly connected to WDO, i.e. a mechanical relay with a coil and mechanical contacts?

What are the electrical parameters of this relay?

And you have read the data sheet, table 4, parameter VIL, and you also understand what R25/R26 do at pin /EN?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
September 1, 2025

@tensaisakuragi06 wrote:

I attach my drawings below and needs your help.


You omitted a key part of the drawing - you haven't shown how your relay is connected!

And, as @Peter BENSCH said, you need to give full details of the relay.

 

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
September 1, 2025

I use the WDO like microcontroller pin to drive, not to the coil. I also attach the relay connection. I put optional resistors to get precaution against if i left the EN floating and did not drive the STWD100. Because some of the parts in datasheet , left float and somewhere if EN remains high for instance. Its total my lack of inexperience of STWD100.

relay connection.png

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
September 1, 2025

If you control /EN with a voltage divider of 1k+1k, the STWD100 will never work because this results in a voltage of VCC/2. However, as shown in table 4 mentioned above, /EN requires a voltage of max. 30% VCC to enable the STWD100. This means that as long as /EN is not activated, WDO cannot be active either.

Incidentally, WDO is an open drain, which is why you have provided R134 as a pull-up. However, this also means that R40 is pointless and can be replaced by a short circuit.

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
September 1, 2025

With your pointer i am not sure i can drive relay with WDO? because i did not see any parameter like Iwdo, max current value of WDO.

Associate III
September 1, 2025

I am plannig to use as 0R on R25 and R26. If IC works with EN floating, i did not put those resistors. To get trigger soruce from WDO, should not i left floating the EN pin? Currently i left the EN pin floating(did not put any resistor on R25 and 26). I will try shorting the R40.

Andrew Neil
Super User
September 1, 2025

@tensaisakuragi06 wrote:

I am planning to use as 0R on R25 and R26.


If you put 0R on R25 and R26 you will short your VCC supply to GND !

AndrewNeil_0-1756722950854.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
September 1, 2025

I was plannig to left floating of EN du to this statement:enable.png

Peter BENSCH
ST Technical Moderator
September 1, 2025

The excerpt from the data sheet already gives you the answer to your last post.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
September 1, 2025

My bad, you re right i did not put any resistor but when writing here, i write as "planning to put 0R". By the way when changing the relay resistor, i am so close to my plan, when everything works well, IC reset itself by the help of WDI. By external pull-ups, i can drive relay at normal conditon. The remaining problem is this: when i adjust my timer to 2 sec, every transition, WDO toggles. I dont want the toggling process (i set up timer to high value to test if IC works). I attach a video related with that. The logic to latch the WDO confuses me.

Andrew Neil
Super User
September 1, 2025

@tensaisakuragi06 wrote:

The remaining problem is this: when i adjust my timer to 2 sec, every transition, WDO toggles. I dont want the toggling process


That seems consistent with what the datasheet says:

AndrewNeil_0-1756725069285.png

AndrewNeil_1-1756725169268.png

 

So the WDO gives a pulse output with a width between 10us and 280ms.

Are you wanting it to stay asserted permanently once the watchdog has "fired" ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
September 1, 2025

If i am not wrong, this situation happens because of my testing way. I think that relay can not toggle if MCU really crash.

Peter BENSCH
ST Technical Moderator
September 1, 2025

Well, the question is, why are you going to all this trouble to control a relay with a watchdog?

A watchdog is there to reset a device (typically an MCU or MPU) when there are no signs of life, thereby bringing the device out of the ‘death zone’. A relay is rather unsuitable as an intermediary. What is being controlled by the relay?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
September 1, 2025

Its depending on the need. I do not want to recover the IC but somehow want to know if is fine or not. I use it for different purpose rather than the actual  aim.

Associate III
September 1, 2025

Relay is used for just give a warning with its led indication.

Andrew Neil
Super User
September 1, 2025

If it's just an LED, why do you need a relay?

The STWD100NY can easily drive an LED directly!

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.