Skip to main content
Visitor II
September 18, 2024
Solved

STW81200 Custom Library

Hello Everyone,
Can anyone help me out !
Currently, I am working with STW81200 RF Synthesizer Module by using the STM32 Controller. I have used STW81200GUI Tool for frequency generation. But I don't want to use the tool anymore. I want to write my own custom  library for frequency generation (50MHz-6GHz) .i.e., Custom Function to generate Ten 32-bit registers of frequency which is ranging from 50MHz t0 6GHz without using the Tool. But I don't know what are all the parameters to consider for frequency generation. Can you help me to create Ten 32-bit registers for frequency (50MHz-6GHz) without using the Tool.
   
regards,
Tarun Bandari.

    This topic has been closed for replies.
    mƎALLEm
    mƎALLEmBest answer
    ST Technical Moderator
    September 18, 2024

    Hello @Tarun_Bandari and welcome to the community,

    In that case you need to read the STW81200 datasheet and you need SPI communication for that.

    SofLit_0-1726655802825.png

    You need to read the registers description and adapt your custom library according to your needs.

     

     

     

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

    2 replies

    mƎALLEm
    mƎALLEmBest answer
    ST Technical Moderator
    September 18, 2024

    Hello @Tarun_Bandari and welcome to the community,

    In that case you need to read the STW81200 datasheet and you need SPI communication for that.

    SofLit_0-1726655802825.png

    You need to read the registers description and adapt your custom library according to your needs.

     

     

     

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
    Tesla DeLorean
    Guru
    September 18, 2024

    Read the data sheet.

    Review other library code and examples.

    Write your own implementation / interpretation of that 

    Test

    Done

     

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..