Skip to main content
RobK1
Associate II
Dec 18, 2025 9:01 AM UTC
Question

STVD works fine with windows 7; W10 64bit I failed to install

Split from Is STM8 recomended for beginners?

Originally in reply to this post.


STVD Version 4.3.12 (August 4, 2017!!) runs fine here on W11.

    3 replies

    Graduate II
    Dec 18, 2025 2:15 PM UTC
    In 2021 I tried to install STVD on W10-64bit and failed. On the other hand, I have Ubuntu Linux next to windows and I installed W7 and STVD on virtualbox there. I didn't try to install it on windows later.
    Graduate
    Dec 22, 2025 4:51 PM UTC

    I guess that VirtualBox is the cause of the problem. I've tried to use STVD on VirtualBox with Windows XP SPII and Cosmic did not request a license as it was on Windows 11 (without VirtualBox).

    Graduate II
    Dec 22, 2025 8:21 PM UTC
    In Windows 10 I installed without virtualbox.