Skip to main content
hg-chen
Associate III
Oct 12, 2004 6:02 AM UTC
Question

STVD with Cosmic and Metrowerks,step by step instruction ?

Posted on October 12, 2004 at 08:02

STVD with Cosmic and Metrowerks,step by step instruction ?

This topic has been closed for replies.

4 replies

hg-chen
hg-chenAuthor
Associate III
Sep 30, 2004 7:24 AM UTC
Posted on September 30, 2004 at 09:24

any brief step by step instrcution to create new workspace,then toolchains path and prohject settings so that build can be succeed?

try using the Cosmic workspace sample in ST7 Software Library 2.0,

the build is failed!
parveen
Associate II
Sep 30, 2004 7:51 AM UTC
Posted on September 30, 2004 at 09:51

Try using Rebuid all option for first time.

For which device you want to create workspace, ST7Library has ready to

use workspace for different devices.

Also configuration files (.mak,.prm and .lkf ) for most of ST7 devices are available at device\cosmic or devices\metrowerks path.

Hope this helps

Thanks and Regards,

PraveenG
nciot
Visitor II
Oct 6, 2004 4:54 AM UTC
Posted on October 06, 2004 at 06:54

Hi Kuni,

you can find more information on how to create a Cosmic, Hiware or Assembler project for STVD7, reading the SofTec Application note AN002, this is the link:

http://www.softecmicro.com/downloads/doc/sft_an002.pdf

Cheers,

Nicola
hg-chen
hg-chenAuthor
Associate III
Oct 12, 2004 6:02 AM UTC
Posted on October 12, 2004 at 08:02

using workspace of ST7LIB2 or ST7FMC download from web site,

in project setting

Maker : Gmake

Maker filename : C:\COSMIC\EVALST7\gmake

but there is no gmake file in my C:\COSMIC\EVALST7

what should I modified in the project setting in order to make the

Build succeeded ?