Skip to main content
remi23
Associate II
Apr 27, 2012 1:50 PM UTC
Question

stvd: one or more breakpoints are not positioned on valid lines

Posted on April 27, 2012 at 15:50

Hi

Here is the bug I found in STVD:

While trying to debug a program I set a breakpoint on a line, load the debugger and bam error:

one or more breakpoints are not positioned on valid lines.

I know this is a valid line, this same breakpoint worked yesterday and before that... I tryed to delete the project files, nothing works

any idea to fix ST software?
    This topic has been closed for replies.

    5 replies

    remi23
    remi23Author
    Associate II
    Apr 27, 2012 1:58 PM UTC
    Posted on April 27, 2012 at 15:58

    OK I just fixed it using my version control software (Toirtoise CVS)

    Reverting all the project file that corrupt themself FOR NO GOOD REASONS

    STVD needs really a fix for that. It is not a new error, this error has been around for years!!!

    Stm32User
    Associate III
    Apr 27, 2012 2:06 PM UTC
    Posted on April 27, 2012 at 16:06

    I have used STVD for many years and never seen the corruption you mention.

    The invalid breakpoint error usually occurs when you set the compiler to a non-debug compatible mode.  Then the source code line is there but the compiler has optimised away the instructions, which is why the breakpoint can't be set 

    nick239955_stm1
    Visitor II
    Apr 25, 2013 9:36 AM UTC
    Posted on April 25, 2013 at 11:36

    I have optimisations turned completely OFF and I get the error also. It never used to happen but now happens all the time. I am going to try creating a new project and importing my source code files.

    clevis
    Visitor II
    Nov 13, 2013 9:06 AM UTC
    Posted on November 13, 2013 at 10:06

     Maybe resulted from the File directory changed!

      �?�能你修改了工程路径�?

    prado
    Visitor II
    Jul 8, 2014 12:38 AM UTC
    Posted on July 08, 2014 at 02:38

    Hello,

    Have you checked if the directory of the files you're trying to set a breakpoint was informed in the field ''Source directories'' on the Debug tab of your project settings?