Skip to main content
anatoli_soltan
Associate
Mar 26, 2011 3:17 AM UTC
Question

STVD displays ''The parameter is incorrect''

Posted on March 26, 2011 at 04:17

Just received my STM8L-Discovery, installed STVD 4.2.1 and Raisonance compiler. Whenever I hit F7, STVD shows this non-descriptive message ''The parameter is incorrect''. After that, the only way to exit the application is to kill it in the Task Manager. I tried it on Win XP and Win 7 (32-bit) with same results.

Does anyone experienced a similar problem?

Thanks for help!

    This topic has been closed for replies.

    35 replies

    tombearlee
    Visitor II
    Mar 28, 2011 8:06 PM UTC
    Posted on March 28, 2011 at 22:06

    I do have the same problem. How can we resolve it?

    Thanks,

    anatoli_soltan
    Associate
    Mar 31, 2011 8:32 PM UTC
    Posted on March 31, 2011 at 22:32

    Would anyone from ST provide help on this issue?

    Thank you!

    napoleoni.jacques
    ST Employee
    Apr 1, 2011 7:56 AM UTC
    Posted on April 01, 2011 at 09:56

    Hello,

    Did you experience this problem whatever the project used or with a particular one?

    Thank you,

    Regards.

    napoleoni.jacques
    ST Employee
    Apr 1, 2011 8:02 AM UTC
    Posted on April 01, 2011 at 10:02

    Hello,

    Please could you provide before application crash the following zip file by the menu:

    Help\Generate Support File...

    Check the path, type a file name, then press OK. After attach the file to a new forum message.

    Also, what is the Raisonance version?

    Thanks and Regards.

    normand
    Associate II
    Apr 4, 2011 6:39 PM UTC
    Posted on April 04, 2011 at 20:39

    We have installed this version 4.2.1 on only 1 of our lab computers with the same result.

    We also have the same issue now with STM8S-Dicovery board witch was ok before with V4.2.0.

    ?????

    Regards

    napoleoni.jacques
    ST Employee
    Apr 5, 2011 8:18 AM UTC
    Posted on April 05, 2011 at 10:18

    Hello,

    Please could you also provide the ''Support file'' and give us the Raisonance version.

    In the meantime, please try to update your Raisonance compiler release. Some modifications of STVD have been done between 4.2.0 and 4.2.1 that are may be not compliant with old Raisonance releases.

    Please check this point and come back to the forum if needed.

    Regards.

    normand
    Associate II
    Apr 5, 2011 7:55 PM UTC
    Posted on April 05, 2011 at 21:55

    We don't use the Resonance compiler but the STAssmebler/Linker There is no sing of the Rsonance compiler in the support file.

    Regards

    napoleoni.jacques
    ST Employee
    Apr 6, 2011 7:31 AM UTC
    Posted on April 06, 2011 at 09:31

    You're posting a message on the topic ''The parameter is incorrect'' and said that you had the same error so I was thinking that you also got ''The parameter is incorrect'' message and used Raisonance too...

    If your request refers to another problem, please detail the issue and give information on the error message...

    Thank you.

    normand
    Associate II
    Apr 6, 2011 1:44 PM UTC
    Posted on April 06, 2011 at 15:44

    OK, should i post a new message for each Tollset we use with STVD 4.2.1 since they all lead to the same issue. Sorry that I have not mentioned the toolset.

    Regards!

    napoleoni.jacques
    ST Employee
    Apr 6, 2011 3:00 PM UTC
    Posted on April 06, 2011 at 17:00

    If we mix all problems with all solutions, I'm not sure this forum will be helpful for anyone. These are basics of support.

    If you're complaining about initial error ''the parameter is incorrect'', you may have an issue with Raisonance and we're suggesting to solve it by updating your Raisonance version.

    Regards