Skip to main content
fggnrc
Associate III
Jan 15, 2010 9:46 AM UTC
Question

STVD 4.1.4 bug (.NOLIST in ASM include files)

Posted on January 15, 2010 at 10:46

STVD 4.1.4 bug (.NOLIST in ASM include files)

    This topic has been closed for replies.

    1 reply

    fggnrc
    fggnrcAuthor
    Associate III
    May 17, 2011 1:07 PM UTC
    Posted on May 17, 2011 at 15:07

    Dear Sirs,

    I found a bug in how the latest STVD release manages ASM include files.

    The attached archieve contains a default project to which I added MyInc.inc

    This file contains only a .NOLIST directive and a #define.

    After the project is successfully built, the simulator (and also my R-Link tool) gives this warning:

    -> warning: remove white-space characters at the end of the last line of the include file

    If I execute the code, there is no way to single-step through the code...

    If I do as the warning suggests, the project can't be built.

    Regards

    EtaPhi

    PS: a workaround is obviously to delete .NOLIST directives...