Skip to main content
Visitor
Nov 19, 2026 8:33 PM UTC
Question

STUSB4531 SCL / SDA leakage when powered down

The STUSB4500 datasheet notes:

  SCL and SDA are pulled down when none of VDD or VSYS is present

This was further clarified in the thread:

  STUSB4500 – I²C Pullup with No VBUS/VDD Applied

  if the STUSB4500 is not supplied (no charger connected), be aware
  that you will get a leakage current on SDA and SCL pins (few hundred
  of µA), it will impact SDA and SCL level (from 3.3V to 2.7V if you
  use 3.3kohms resistors).

I don't see any mention of the issue in the STUSB4531 datasheet
so I'm not clear if the same issue is present.

Likewise what is the leakage of the ALERT pin when the STUSB4531 is
powered down?

As a follow up question, one solution to the leakage might be to
use something like a PCA9617A to isolate the STUSB4531 ... can the
VREG_2V7 be used to power port A along with the pullups for port A?
The STUSB4531 datasheet doesn't mention the 2V7 LDO current capabilities.