Skip to main content
Visitor
July 15, 2026
Question

STSPIN32G4-ADC-error

  • July 15, 2026
  • 0 replies
  • 17 views

When using the STSPIN32G4 chip, the ADC uses an external resistor for non-inverting amplification to determine the value, but in reality, the ADC-OUT output is always at the maximum of its internal LDO. Changing the external feedback resistor can't change the output value of its op-amp. What could be the reason for this? Also, the voltage difference on the non-inverting side of the three op-amps is inconsistent: two are 0.27, and one is 0.35. I’d like to ask the experts for advice.