Skip to main content
Associate
October 15, 2025
Question

Strange behavior on open-drain output mode for blue pill (STM32F103C8T6)

Guys, I need to put 5V on a pin. For this, I configured my pin as an open-drain output with a pull-up resistor (10k) between the pin and the 5V line. I checked the 5V-tolerant pins in the Blue Pill datasheet and tested many of them, but the conclusion is always the same: the output is 3.7V when the pin is in high impedance. I used Keil uVision to write my code in C (at startup, I only used CMSIS and DEVICE for pre-configuration). My code is below. I used PB10 as a reference.

#include "stm32f10x.h"

int main(){
 RCC->APB2ENR |= (1 << 3); // Clock for GPIOB

 // Open-drain output and HIGH impedance PB10
 GPIOB->CRH &= ~(0b1111 << 8); // Cleaning bits
 GPIOB->CRH |= (0b0111 << 8); // Setting up bits

 GPIOB->ODR |= (1 << 10); // HIGH impedance
};
 
Could you guys please tell me what I did wrong? 

Edited to apply source code formatting - please see How to insert source code for future reference.

This topic has been closed for replies.

7 replies

TDK
October 15, 2025

Maybe the overwhelmingly likely counterfeit chip on the board doesn't have 5 V tolerant pins.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Luki_GrinAuthor
Associate
October 15, 2025

Thanks for your comment! I didn't think it was a clone, as the debugger with STM32CubeIDE worked perfectly fine. However, after checking some IDs, I found very strange values, so it's probably fake =(

Peter BENSCH
ST Technical Moderator
October 15, 2025

You have (at least) made two mistakes:

  • You are using a so-called Blue Pill that has only been used with counterfeits for years (and you are asking for a solution for the counterfeit in the forum of the original manufacturer).

  • You are confusing 5V tolerance (of an input) with 5V capability of an output

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Luki_GrinAuthor
Associate
October 15, 2025

Thanks for the clarification, Peter. I'm new to the world of microcontrollers, and I'm diving into bare metal to understand how things really work. Didn't know there were clones. I will probably move to a NUCLEO one in the future (to avoid spending many hours on these bugs). 

"You are confusing 5V tolerance (of an input) with 5V capability of an output" --> Could you explain what you mean? I know the output voltage on a pin is normally 3.3V, but if I configure the output as open-drain (high impedance) and connect a pull-up resistor to it, I can get higher values of voltage, right? 

Peter BENSCH
ST Technical Moderator
October 15, 2025

This depends on:

  • whether the specific GPIO has an alternative analogue function
  • and, as mentioned, whether it is an original or a counterfeit.

Details on GPIO behaviour can be found for the original device in the data sheet and in the Reference Manual RM0008.

Hope that helps?

Regard
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.