Skip to main content
aled
Associate
Oct 16, 2009 7:35 PM UTC
Question

STR912FA Sleep Mode - Hangs!

Posted on October 16, 2009 at 21:35

STR912FA Sleep Mode - Hangs!

This topic has been closed for replies.

11 replies

omniprintinc
Associate
May 17, 2011 7:47 AM UTC
Posted on May 17, 2011 at 09:47

Hello ly_liuyang_ly

From what I read in the ST application note AN2633, there should be 3 ''dummy'' instructions after executing the command to enter a low power mode if the system is running from the 32 kHz clock as your appears to be. In your call to the ST library function SCU_EnterSleepMode(), after the sleep mode bit is set in the SCU_PWRMNG register, there is a BX LR instruction to return from the function call. Likewise, there are likely four instructions to clear the WIU Pending Register:

WIU->PR = 0xFFFFFFFF;

LDR R0,WIU_Addr

LDR R0,[R0, #+0]

MVN R1,#+0

STR R1,[R0, #+12]

That is five instruction right away before your CPU even gets to the NOPs. Shouldn't it already be in a low power state at this point. If it is, your CPU will never execute the remainder of the instructions

Quote:

/* Dummy instructions

Execution of N=12 dummy instructions. This number depends on

the ratio between CPU clock frequency and the oscillator input

frequency(Please refer to the STR91xFA reference manual).

For fcpuclk = 32.768Khz, N=3 */

__nop(); __nop(); __nop();

/*Switch to oscillator as clock source after wake up*/

if (y > 25)

{ // MCLK by PLL

while(!(SCU->SYSSTATUS&SCU_FLAG_LOCK)); /*Wait PLL to lock*/

SCU_MCLKSourceConfig(SCU_MCLK_PLL); // restore clock, if it woke up...

} else SCU_MCLKSourceConfig(SCU_MCLK_OSC);

SetLED(0);

// clear RTC alarm and enable WIU interrupt

RTC_ITConfig(RTC_IT_Alarm, DISABLE);

RTC_AlarmCmd(DISABLE);

RTC_ITConfig(RTC_IT_Per, ENABLE);

VIC_ITCmd(WIU_ITLine, ENABLE);

OS_EXIT_CRITICAL(); // enabled interrupts globally

before it enables the interrupts to allow the CPU to be woken up from the low power mode.

Please let me know if I am not understanding this correctly.

Also, can anyone from ST comment on the AN2633 section 1.4.5 where it says

Quote:

Once Idle mode or Sleep mode are entered by writing the PWR_MODE[2:0] bits in the Power management register (SCU_PWRMNG) it takes about 12 crystal oscillator cycles (X1_CPU input frequency) for the device before stopping the execution.

How does one code about 12 cycles worth of instructions?