Skip to main content
stefangrohmann9
Associate
Jan 23, 2007 6:07 AM UTC
Question

STR912F44W CAN receiver not working

Posted on January 23, 2007 at 07:07

STR912F44W CAN receiver not working

This topic has been closed for replies.

2 replies

stefangrohmann9
Associate
May 17, 2011 7:35 AM UTC
Posted on May 17, 2011 at 09:35

The problem is: STR912F44W CAN node in silent-mode.

CAN-TX on port 5.1 is working (in Loopback-mode) but the receiver is not working in all modes - also not in silent mode. FI2 is selected for RX buffer. Acceptance filter is set to the full range like the example does. Interrupt is enabled scu on port 5 is enabled - but no int occures. Any ideas? :o

mehdi239955
Visitor II
May 17, 2011 7:35 AM UTC
Posted on May 17, 2011 at 09:35

hi Softy,

>CAN-TX on port 5.1 is working (in Loopback-mode) but the receiver is not working in all modes

Can you send the configuration (CAN and GPIO)you're using ?

it seems that the GPIO configuration is not right because the loopback-mode is working ;)

Waiting for your response

best regards.

:D