Skip to main content
hjn
Associate II
Jun 20, 2009 4:09 AM UTC
Question

STR912 Flash Loader Demonstrator program

Posted on June 20, 2009 at 06:09

STR912 Flash Loader Demonstrator program

This topic has been closed for replies.

3 replies

lloydepowell
Associate
May 17, 2011 7:58 AM UTC
Posted on May 17, 2011 at 09:58

I am using the AN2475.zip found at the right under Application Notes in

http://www.st.com/mcu/devicedocs-STR911FAM47.html

hjn
hjnAuthor
Associate II
May 17, 2011 7:58 AM UTC
Posted on May 17, 2011 at 09:58

Hi all,

In the pdf document called Application note AN2475 (page 8) ST wrote.

ST provides a free Flash loader utility allowing the program of the STR91xFA internal Flash Bank0 using an IAP driver to be loaded in the Flash Bank1.

Please, I can't find that Flash Loader program, can anybody help me here.

In the AN2475 document (page 30) I can see that they can select a CPU target : STR91xFAWy4

I found a Flash Loader Demonstrator v1.3 for the STM32F10xxxx, but I can't use that.

Hope someone here can help me to find the Flash Loader Demonstrator for

STR91x.

Thanks

Hans

woshilongsan
Visitor II
May 17, 2011 7:58 AM UTC
Posted on May 17, 2011 at 09:58

HI! lloydepowell

I am running the IAP programmer as detailed in AN2475 and PM0020 to load my app into Bank 0. Bank 1 is the boot. BBSR and NBBSR are set correctly for 512k bank 0 and 32k Bank 1. The programing is successful in the first 8192 bytes. But at address x82000, it fails to program. Any ideas?

Do you have encountered this problem?

help me

thanks.