Skip to main content
s_bhujbal
Associate III
Mar 23, 2009 5:06 AM UTC
Question

STR9-JTAG Prog. Tool

Posted on March 23, 2009 at 06:06

STR9-JTAG Prog. Tool

This topic has been closed for replies.

3 replies

s_bhujbal
s_bhujbalAuthor
Associate III
May 17, 2011 7:58 AM UTC
Posted on May 17, 2011 at 09:58

Dear All,

We are working on STR9 - IAP.

For changing Boot Bank order & loading IAP driver we are using RFlasher.

Then we uses ST Flash Loader for programming Application

in Bank0 through UART0.

Uptill this everything is OK.

But Aplication is not running.

If we want to reorder the Boot Banks, how should we do it ?

Presently we are not getting any setting in RFlasher for it.

s_bhujbal
s_bhujbalAuthor
Associate III
May 17, 2011 7:58 AM UTC
Posted on May 17, 2011 at 09:58

Thank You, VincentC,

Now I am able to programme & boot required bank if I programmed

those from Rflasher. :D

I downloaded my Application in Bank0 through JTAG & after that

ST IAP driver in Bank1 ( with booting from it ).

Now whenever STR9 boots, firat it runs IAP driver.

If push button is not pressed, it starts Application Code

correctly. :D

If push button is pressed then it start UART programming mode.

I also abled to download application code through STFlasher & UART.

ST Flasher ''Invalid Address'' error , if I doanloadhex file

in it. :-[

Therefore I converted same hex file to bin & downloaded it through

ST Flasher & UART successfully, but when I restarts STR9 after it,

application code doesn't works . :-[

What should be done for it ?

Please help,

Sachin Bhujbal

[ This message was edited by: s_bhujbal on 23-03-2009 10:37 ]

[ This message was edited by: s_bhujbal on 23-03-2009 10:38 ]

vincentchoplin9
Visitor II
May 17, 2011 7:58 AM UTC
Posted on May 17, 2011 at 09:58

Hi,

Please see this thread on the Raisonance forum:

http://raisonance-forum.xsalto.com/viewtopic.php?id=2741

That will tell you how to configure RFlasher for programming the Configuration, and the CSX bit that is inside it.

Best Regards,

Vincent