Skip to main content
nospam2
Associate II
Oct 23, 2006 12:11 PM UTC
Question

STR9 FreeRTOS port with WEB server

Posted on October 23, 2006 at 14:11

STR9 FreeRTOS port with WEB server

This topic has been closed for replies.

13 replies

hd2
Associate
May 17, 2011 7:30 AM UTC
Posted on May 17, 2011 at 09:30

To make the FreeRTOS demo link without removing any source, you can change the optimizations to Maximum for size, and reduce the library options to minimum printf and scanf. Then it's just BARELY small enough to link. And it still runs!

yuantuh
Visitor II
May 17, 2011 7:30 AM UTC
Posted on May 17, 2011 at 09:30

Hi Tony,

I got the same problem. From error message I guess the demo project would generate more than 32K code which is beyond KickStart 32K (0x8000)limitation.

nospam2
nospam2Author
Associate II
May 17, 2011 7:30 AM UTC
Posted on May 17, 2011 at 09:30

This point was recently raised on the support forum. See the thread:

http://sourceforge.net/forum/forum.php?thread_id=1592185&forum_id=382005

My intention was to keep the demo under the 32K limit - but I did not take into account the const data used by the html pages that are built into the binary. The executable code is 29K (ish), but then there is 6K of HTML pages.

You will have to remove some of the demo files and/or replace the html pages with a simple one pager as a starter. See more info in the thread referenced above.

Sorry for inconvenience. I will update the demo in the download accordingly.

Regards.