Skip to main content
gedass2000
Associate II
November 21, 2007
Question

STR752 system memory bootloader

  • November 21, 2007
  • 11 replies
  • 2524 views
Posted on November 21, 2007 at 12:46

STR752 system memory bootloader

This topic has been closed for replies.

11 replies

gedass2000
Associate II
November 13, 2006
Posted on November 13, 2006 at 18:15

Hi all,

seems like I deleted bootloader sector from system memory.Is it possible to get file for programming this flash zone ?

mohamed23
Associate
November 14, 2006
Posted on November 14, 2006 at 12:07

Hello,

The STR75x bootloader can not be deleted nor programmed by User or by any

programming tool in the Market. This can be done only in STMicroelectronics.

For sure, you have something wrong in your configuration,

Could you please check your Boot mode and if you are booting from

the right SystemMemory Mode. For more details you can refer to

''AN2430 : STR75x SystemMemory boot mode''

With best regards,

Rave

gedass2000
Associate II
November 14, 2006
Posted on November 14, 2006 at 13:31

Quote:

On 14-11-2006 at 16:37, Anonymous wrote:

Hello,

The STR75x bootloader can not be deleted nor programmed by User or by any

programming tool in the Market. This can be done only in STMicroelectronics.

For sure, you have something wrong in your configuration,

Could you please check your Boot mode and if you are booting from

the right SystemMemory Mode. For more details you can refer to

''AN2430 : STR75x SystemMemory boot mode''

With best regards,

Rave

Hi,

it is very strange... I set BOOT0 = 1 (Vcc) , BOOT1 = 0 (GND) , GPIO0.4 = 0 (Gnd) and after RESET I send 0x7F to comport0 . I have to get back 0x75 but don't get any characters.I am using Keil demo board.

kaouther
Associate II
November 16, 2006
Posted on November 16, 2006 at 07:13

Hello,

That's stange! What is the date code of the STR752 chip on Keil board? just send us all infos written on STR752 package.

Thanks.

gedass2000
Associate II
November 16, 2006
Posted on November 16, 2006 at 08:19

Quote:

On 16-11-2006 at 11:43, Anonymous wrote:

Hello,

That's stange! What is the date code of the STR752 chip on Keil board? just send us all infos written on STR752 package.

Thanks.

MCBSTR750 Vers.1

MCU: STR750FV2T6 Z

22 024 V6

MLT 22 630

michael7
Visitor II
November 22, 2006
Posted on November 22, 2006 at 19:59

I'm having this same identical problem on an IAR STR750-SK rev B evaluation board, although I encountered it with a virgin board (no chance of accidentally erasing anything.)

My STR750 Chip says:

STR750FV2T6

Z

22 024 VG

MLT 22 630

Which is identical to the previous posters, except I think they may have misread a ''G'' as a ''6''...

gedass2000
Associate II
November 23, 2006
Posted on November 23, 2006 at 06:03

Quote:

On 23-11-2006 at 00:29, Anonymous wrote:

I'm having this same identical problem on an IAR STR750-SK rev B evaluation board, although I encountered it with a virgin board (no chance of accidentally erasing anything.)

My STR750 Chip says:

STR750FV2T6

Z

22 024 VG

MLT 22 630

Which is identical to the previous posters, except I think they may have misread a ''G'' as a ''6''...

Hi,

I got a message from ST that this revision don't has properly working bootloader

:-[

mohamed23
Associate
November 23, 2006
Posted on November 23, 2006 at 15:33

Hi all,

Yes, all the starter kits from IAR,Keil, Hitex, Raisonnance and ST

already you are using have an early version of silicon that does not contain the bootloader as described in the Application Note.

You have to contact ST Sales to get the new samples shipped from the begining of September when the STR750 product is launched and try to rework the chip in your board.

With best regards :)

kaouther
Associate II
December 5, 2006
Posted on December 05, 2006 at 04:56

Hi All,

Please find the answer to these questions in the A.N2430 ''STR75x SystemMemory boot mode''. There is a detailed section for the bootloader availability on the devices. I attached the A.N , also available on the web site.

With Best Regards,

________________

Attachments :

AN2430.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtRS&d=%2Fa%2F0X0000000aQ5%2F04zP0A3dXtgZoJYnlLAUtgtstQw.UmeQtykFEIFa1Lg&asPdf=false
alessandro2399
Visitor II
November 16, 2007
Posted on November 16, 2007 at 11:18

At this time is there any Win PC tool for STR75x flash programming through its system memory bootloader? Or shall I make it by myself?

Best Regards