Skip to main content
ariel
Associate
Jun 4, 2008 12:41 PM UTC
Question

STR751FR0 with a single supply of 5 Volts

Posted on June 04, 2008 at 14:41

STR751FR0 with a single supply of 5 Volts

This topic has been closed for replies.

3 replies

ariel
arielAuthor
Associate
May 19, 2008 8:54 AM UTC
Posted on May 19, 2008 at 10:54

In the power schemes in the STR751FR0 data sheet it is written that there are four power schemes ,single 3.3V or 3.3V + 1.8 V or single 5 V or 5V+1.8V.

But in the table of the same data sheet HEREBY ATTACHED it is written only 3.3V supply.

My question is:

Can I power the STR751FR0 with a single supply of 5 Volts.

[ This message was edited by: ariel.rachminov on 19-05-2008 14:27 ]

[ This message was edited by: ariel.rachminov on 19-05-2008 14:35 ]

[ This message was edited by: ariel.rachminov on 19-05-2008 14:38 ]

[ This message was edited by: ariel.rachminov on 19-05-2008 14:38 ]

________________

Attachments :

STR751FR0_data_sheet_Page.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtRN&d=%2Fa%2F0X0000000aQ4%2FPgC_0f.Mw4M0Tpou6.lPFDE7ygFqPL6PSxxcV4iUtyU&asPdf=false
jgoril
Associate III
May 20, 2008 3:54 AM UTC
Posted on May 20, 2008 at 05:54

Few pages later there is a caution: ''When powered by 5.0V, the USB peripheral cannot operate.''

So 5.0V supply for STR751 and STR750 is with restricted use only...

kaouther
Associate II
Jun 4, 2008 12:41 PM UTC
Posted on June 04, 2008 at 14:41

Yes there are four power schemes for the STR75x devices. With the wide range of STR75x part number, you can choose the suitable part number for your application. The STR751 is the one integrating the USB and recommend the 3.3V power supply since with 5.0V the USB is not available. if you don't use the USB in your application, you can choose either the STR755 or STR752. ;)