Skip to main content
pratibha
Associate
Jan 9, 2007 10:56 AM UTC
Question

str710fz2 Programming by RIDE error

Posted on January 09, 2007 at 11:56

str710fz2 Programming by RIDE error

This topic has been closed for replies.

2 replies

pratibha
pratibhaAuthor
Associate
Jan 6, 2007 8:49 AM UTC
Posted on January 06, 2007 at 09:49

Hi,

I am using RIDE BN version 746 & RFlasher to program STR710FZ2. I was able to program so far. I am booting from internal FLASH, using ST libraries.

1. Today it started giving message like

''Timeout Expired while Trying to reset Target'' for any commands

like erase, blankcheck etc. But it can communicate with target &

reads device id. Why is it?

2. I have enabled UART3's TxEmpty interrupt and it is doing transmission

fine(continuously). I am using ST library functions to init or

configure device. But

I am getting non-stop TxEmpty interrupts even if i dont write anything

to TxBUFR register. I even trying to clear pending bit with '1' but of

no use.

3. I am using EMI BANK0 to connect to CompactFlash but not yet soldered

CF. If I only read, i dont see any RDn or CS0 signal on scope but if

add some write instruction, i can see both RDn, WRn, CS0. Why is it?

Please help.

Thanks in advance.. :-[

vincentchoplin9
Visitor II
Jan 9, 2007 10:56 AM UTC
Posted on January 09, 2007 at 11:56

Hi,

I answered the first question on the Raisonance forum:

http://www.raisonance.com/Forum/phorum-3.3.2b2/read.php?f=1&i=6822&t=6822

I don't know the answers to the two other points...

Best Regards,

Vincent