Skip to main content
thierry239955_st
Associate
Aug 8, 2005 5:48 AM UTC
Question

STPC Linux and WinCE.net loaders available for free - full source code

Posted on August 08, 2005 at 07:48

STPC Linux and WinCE.net loaders available for free - full source code

This topic has been closed for replies.

11 replies

thierry239955_st
Associate
Aug 8, 2005 5:48 AM UTC
Posted on August 08, 2005 at 07:48

Hi Jay,

Flash card are traditionally connected to the IDE controller and would require to initialize this controller before to access it. You also need to transfer data to the RAM before to execute the code as flash card doesn't support eXecute-in-Place.

This two operations (IDE intitialization + transfer to the RAM) are both done by the bootloader itself... that then need to be stored in another location.

The usual way is to store the bootloader in a standard NOR flash and the rest of the system in the flash card. I unfortunatly don't see any better solution...

Farfalla