Skip to main content
Associate
June 23, 2025
Question

`stmmac` driver error: MAC to MAC communication

Hi there,

I am trying to use the stmmac driver the .dtsi here to connect two GMII MAC components.

gmac0 and gmac1 are activated as followed in a separate .dts file - note that gmac2 is configured and confirmed to be working prior to this:

&gmac0 {
	status = "okay";
	mac-mode = "gmii";
	phy-mode = "gmii";
	max-speed = <1000>;
	max-frame-size = <9000>;
	fixed-link {
	 speed = <1000>;
 full-duplex;
	};
};

&gmac1 {
	status = "okay";
	mac-mode = "gmii";
	phy-mode = "gmii";
	max-speed = <1000>;
	max-frame-size = <9000>;
	fixed-link {
	 speed = <1000>;
 full-duplex;
	};
};

&gmac2 {
	status = "okay";
	phy-mode = "rgmii-id";
	phy-handle = <&emac2_phy0>;

	max-frame-size = <9000>;

	mdio0 {
		#address-cells = <1>;
		#size-cells = <0>;
		compatible = "snps,dwmac-mdio";
		emac2_phy0: ethernet-phy@0 {
			reg = <1>;
		};
	};
};

When I then boot linux, I find the following error messages:

root@localhost:~# dmesg | grep "socfpga-dwmac"
[ 1.433914] socfpga-dwmac 10810000.ethernet: Adding to iommu group 0
[ 1.440789] socfpga-dwmac 10810000.ethernet: IRQ eth_wake_irq not found
[ 1.447387] socfpga-dwmac 10810000.ethernet: IRQ eth_lpi not found
[ 1.453610] socfpga-dwmac 10810000.ethernet: RX VLAN HW Stripping
[ 1.459766] socfpga-dwmac 10810000.ethernet: SMTG Hub Cross Timestamp supported
[ 1.467356] socfpga-dwmac 10810000.ethernet: User ID: 0x76, Synopsys ID: 0x31
[ 1.474476] socfpga-dwmac 10810000.ethernet: XGMAC2
[ 1.479421] socfpga-dwmac 10810000.ethernet: DMA HW capability register supported
[ 1.486867] socfpga-dwmac 10810000.ethernet: RX Checksum Offload Engine supported
[ 1.494311] socfpga-dwmac 10810000.ethernet: COE Type 1
[ 1.499510] socfpga-dwmac 10810000.ethernet: TX Checksum insertion supported
[ 1.506522] socfpga-dwmac 10810000.ethernet: TSO supported
[ 1.511980] socfpga-dwmac 10810000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 1.519954] socfpga-dwmac 10810000.ethernet: device MAC address ca:3e:cc:fb:1a:6f
[ 1.527409] socfpga-dwmac 10810000.ethernet: Enabled L3L4 Flow TC (entries=16)
[ 1.534597] socfpga-dwmac 10810000.ethernet: Enabled RFS Flow TC (entries=10)
[ 1.541696] socfpga-dwmac 10810000.ethernet: TSO feature enabled
[ 1.547672] socfpga-dwmac 10810000.ethernet: SPH feature enabled
[ 1.553647] socfpga-dwmac 10810000.ethernet: TX COE limited to 2 tx queues
[ 1.560490] socfpga-dwmac 10810000.ethernet: Using 40/40 bits DMA host/device width
[ 1.568244] socfpga-dwmac 10810000.ethernet (unnamed net_device) (uninitialized): failed to setup phy (-22)
[ 1.578069] socfpga-dwmac: probe of 10810000.ethernet failed with error -22
[ 1.585185] socfpga-dwmac 10820000.ethernet: Adding to iommu group 1
[ 1.591958] socfpga-dwmac 10820000.ethernet: IRQ eth_wake_irq not found
[ 1.598547] socfpga-dwmac 10820000.ethernet: IRQ eth_lpi not found
[ 1.604742] socfpga-dwmac 10820000.ethernet: RX VLAN HW Stripping
[ 1.610871] socfpga-dwmac 10820000.ethernet: SMTG Hub Cross Timestamp supported
[ 1.618262] socfpga-dwmac 10820000.ethernet: User ID: 0x76, Synopsys ID: 0x31
[ 1.625371] socfpga-dwmac 10820000.ethernet: XGMAC2
[ 1.630312] socfpga-dwmac 10820000.ethernet: DMA HW capability register supported
[ 1.637756] socfpga-dwmac 10820000.ethernet: RX Checksum Offload Engine supported
[ 1.645200] socfpga-dwmac 10820000.ethernet: COE Type 1
[ 1.650400] socfpga-dwmac 10820000.ethernet: TX Checksum insertion supported
[ 1.657412] socfpga-dwmac 10820000.ethernet: TSO supported
[ 1.662870] socfpga-dwmac 10820000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 1.670837] socfpga-dwmac 10820000.ethernet: device MAC address 9a:56:d9:98:64:37
[ 1.678288] socfpga-dwmac 10820000.ethernet: Enabled L3L4 Flow TC (entries=16)
[ 1.685476] socfpga-dwmac 10820000.ethernet: Enabled RFS Flow TC (entries=10)
[ 1.692576] socfpga-dwmac 10820000.ethernet: TSO feature enabled
[ 1.698551] socfpga-dwmac 10820000.ethernet: SPH feature enabled
[ 1.704526] socfpga-dwmac 10820000.ethernet: TX COE limited to 2 tx queues
[ 1.711367] socfpga-dwmac 10820000.ethernet: Using 40/40 bits DMA host/device width
[ 1.719030] socfpga-dwmac 10820000.ethernet (unnamed net_device) (uninitialized): failed to setup phy (-22)
[ 1.728811] socfpga-dwmac: probe of 10820000.ethernet failed with error -22
[ 1.735813] socfpga-dwmac 10830000.ethernet: Adding to iommu group 2
[ 1.742511] socfpga-dwmac 10830000.ethernet: IRQ eth_wake_irq not found
[ 1.749095] socfpga-dwmac 10830000.ethernet: IRQ eth_lpi not found
[ 1.755277] socfpga-dwmac 10830000.ethernet: RX VLAN HW Stripping
[ 1.761389] socfpga-dwmac 10830000.ethernet: SMTG Hub Cross Timestamp supported
[ 1.768798] socfpga-dwmac 10830000.ethernet: User ID: 0x76, Synopsys ID: 0x31
[ 1.775904] socfpga-dwmac 10830000.ethernet: XGMAC2
[ 1.780844] socfpga-dwmac 10830000.ethernet: DMA HW capability register supported
[ 1.788288] socfpga-dwmac 10830000.ethernet: RX Checksum Offload Engine supported
[ 1.795732] socfpga-dwmac 10830000.ethernet: COE Type 1
[ 1.800930] socfpga-dwmac 10830000.ethernet: TX Checksum insertion supported
[ 1.807942] socfpga-dwmac 10830000.ethernet: TSO supported
[ 1.813399] socfpga-dwmac 10830000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 1.821365] socfpga-dwmac 10830000.ethernet: Enabled L3L4 Flow TC (entries=16)
[ 1.828554] socfpga-dwmac 10830000.ethernet: Enabled RFS Flow TC (entries=10)
[ 1.835654] socfpga-dwmac 10830000.ethernet: TSO feature enabled
[ 1.841629] socfpga-dwmac 10830000.ethernet: SPH feature enabled
[ 1.847605] socfpga-dwmac 10830000.ethernet: TX COE limited to 2 tx queues
[ 1.854445] socfpga-dwmac 10830000.ethernet: Using 40/40 bits DMA host/device width
[ 2.448680] socfpga-dwmac 10830000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 2.457891] socfpga-dwmac 10830000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-1
[ 2.467051] socfpga-dwmac 10830000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-2
[ 2.476248] socfpga-dwmac 10830000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-3
[ 2.485428] socfpga-dwmac 10830000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-4
[ 2.494627] socfpga-dwmac 10830000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-5
[ 2.503864] socfpga-dwmac 10830000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-6
[ 2.513108] socfpga-dwmac 10830000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-7
[ 2.589649] socfpga-dwmac 10830000.ethernet eth0: PHY [stmmac-2:01] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL)
[ 2.600063] socfpga-dwmac 10830000.ethernet eth0: No Safety Features support found
[ 2.607619] socfpga-dwmac 10830000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 2.616428] socfpga-dwmac 10830000.ethernet eth0: registered PTP clock
[ 2.623199] socfpga-dwmac 10830000.ethernet eth0: FPE workqueue start
[ 2.629622] socfpga-dwmac 10830000.ethernet eth0: configuring for phy/rgmii-id link mode
[ 6.724299] socfpga-dwmac 10830000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
...
[ 12.301005] socfpga-dwmac 10810000.ethernet: Failed to reset the dma
[ 12.307534] socfpga-dwmac 10810000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[ 12.322809] socfpga-dwmac 10810000.ethernet eth0: __stmmac_open: Hw setup failed
[ 12.666819] socfpga-dwmac 10820000.ethernet: Failed to reset the dma
[ 12.673381] socfpga-dwmac 10820000.ethernet eth1: stmmac_hw_setup: DMA engine initialization failed
[ 12.684623] socfpga-dwmac 10820000.ethernet eth1: __stmmac_open: Hw setup failed

Does anyone have some experience with this sort of issue?

 

Many thanks,

K

 

This topic has been closed for replies.

2 replies

Peter BENSCH
ST Technical Moderator
June 23, 2025

Welcome @K606, to the community!

Apart from the name of the driver, I don't see any reference to nor any device from STMicroelectronics. Wouldn't it make more sense to contact the maintainer of the repository on this topic (formerly Altera, now Silver Lake)?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
K606Author
Associate
June 23, 2025

Hi @Peter BENSCH 

Thanks for the quick reply - yes I asked them also; but thought that it might be worth asking here as it seemed like a good idea to ask the originators of the tech

Kind Regards,

K