Skip to main content
ptsmith
Associate
Jun 24, 2009 6:15 AM UTC
Question

STM8S208 external clock

Posted on June 24, 2009 at 08:15

STM8S208 external clock

    This topic has been closed for replies.

    2 replies

    mozra27
    Visitor II
    May 17, 2011 1:03 PM UTC
    Posted on May 17, 2011 at 15:03

    Hi Paul,

    Yes, you are right the minimum value for fADC is 1MHz can by a prescaled fMASTER clock. The prescaling factor of the clock depends on the SPSEL[2:0] bits in the ADC_CR1 register.

    Regards

    mozra

    ptsmith
    ptsmithAuthor
    Associate
    May 17, 2011 1:03 PM UTC
    Posted on May 17, 2011 at 15:03

    I would like to run an STM8S208RBT6 from an external 1 Mhz clock. However, it appears that if I do this the ADC cannot be used since the ADC requires at least a 1 MHz clock, and the minimum ADC clock prescale ratio is /2 from fMASTER.

    So, am I correct that in order to use the ADC, the minimum external clock is 2 MHz?

    Paul Smith

    Indiana University Physics