Skip to main content
jimb
Associate
Dec 10, 2009 11:59 AM UTC
Question

STM8S105 Flash Read/Write Access Speed (sanity check for slow access)

Posted on December 10, 2009 at 12:59

STM8S105 Flash Read/Write Access Speed (sanity check for slow access)

    This topic has been closed for replies.

    3 replies

    mozra27
    Visitor II
    May 17, 2011 1:06 PM UTC
    Posted on May 17, 2011 at 15:06

    Hi

    tprog: Standard programming time(including erase) for byte/word/block (1 byte/4 bytes/128 bytes) = 6.6 ms

    Regards

    mozra

    jimb
    jimbAuthor
    Associate
    May 17, 2011 1:06 PM UTC
    Posted on May 17, 2011 at 15:06

    All,

    Re: Answer to my question

    1) Reading flash does not require the unlock

    2) Reading flash is fast -0 microseconds as expected

    3) The STM8S has the RWW ability so to write one byte is very fast if you only write one byte and move to other code functions

    4) In the STM8S to write two bytes you move from micro seconds to milliseconds

    jimb
    jimbAuthor
    Associate
    May 17, 2011 1:06 PM UTC
    Posted on May 17, 2011 at 15:06

    Operation: 1 byte write takes 3.6ms - see code sequence below

    FLASH_Unlock(FLASH_MEMTYPE_DATA);

    FLASH_EraseByte(flash_address);

    FLASH_ProgramByte(flash_address, value);

    FLASH_Lock(FLASH_MEMTYPE_DATA);

    return(value);

    Operation: 1 byte read takes 3 ms - see code sequence below

    FLASH_Unlock(FLASH_MEMTYPE_DATA);

    value = FLASH_ReadByte(flash_address);

    FLASH_Lock(FLASH_MEMTYPE_DATA);

    return(value);

    Setup of clk

    HSI is 16Mhz

    Fcpu is 4Mhz

    Question

    1) Should the unlock/erase/write/lock cycle take approximately 3.6ms

    2) Should the unlock/read/lock cycle take approximately 3.0ms - seems very long

    3) To read the data memory flash do I need to unlock the flash