Skip to main content
JRubi.1958
Visitor II
December 4, 2019
Question

STM8S103K3T6 supply

Hello,

​

I'm designing a new board with a STM8 CPU.

Before, I'm doing a several previous tests.

​

I want to supply with 3.3V the MCU but I found that it works very well with 5V but in the other hand with 3.3V it doesn't work.

​

I checked VCAP voltage, while supplied with 5V I measured right value, 1.8V (core voltage) but if I down the power below 4V the voltage at this pin drops to 0V and, therefore, it doesn't work.

​

The datasheet states voltage can be from 2.95V to over 5V.

​

Any idea?

​

Thank you.​

    This topic has been closed for replies.

    1 reply

    Cristian Gyorgy
    Associate II
    December 17, 2019

    There is something else there, causing it "not to work". Any STM8 will do more than fine with 3.3V.

    Try to give some info on the schematics.