Skip to main content
e_zhui2
Associate
May 3, 2010 9:25 AM UTC
Question

STM8S103F3 PB5/SDA behaves incorrect when used as GPIO

Posted on May 03, 2010 at 11:25

STM8S103F3 PB5/SDA behaves incorrect when used as GPIO

    This topic has been closed for replies.

    4 replies

    mozra272
    Visitor II
    May 17, 2011 1:08 PM UTC
    Posted on May 17, 2011 at 15:08

    Hi Dennis,

    The I2C pins are configured as true open-drain I/O internally, (P-buffer and protection diode to VDD are not implemented) so is not possible to use them as output pins

    can you please check with external pull-up 4.7k on these I/O.

    Regards

    mozra

    jeffrey23
    Associate III
    May 17, 2011 1:08 PM UTC
    Posted on May 17, 2011 at 15:08

    Hi Dennis,

    May I use STM8S103F3 PD5/PD6 as I2C SCL/SDA pins (bit-banging approach) ?

    Does it mean that I need to switch their configuration according to I2C

    Read/Write modes ?

        // Setup Port D

        /*

        [2]101

               7 6 5 4 3 2 1 0

               | | | | | | | |

               | | |___________ SCL (Output)     Push pull output

               | |_____________ SDA (I/O   )     Push pull output

        DDR    0 1 1 0 0 0 0 0

        CR1    0 1 1 0 0 0 0 0

        CR2    0 0 0 0 0 0 0 0

        */

        GPIOD->DDR = 0x70;

        GPIOD->CR1 = 0x70;

        GPIOD->CR2 = 0x00;

     Does the STM8S103F3 support 8051 MCU quasi-bidirection mode ?

    e_zhui2
    e_zhui2Author
    Associate
    May 17, 2011 1:08 PM UTC
    Posted on May 17, 2011 at 15:08

    Thanks, Mozra.

    I am not using the I2C pin to drive 74AC164M now, but with other normal GPIOs. Everything is all right.

    But I am still using the I2C pins(GPIO mode) to drive other components, currently they work ok. Concerning to your reply ''The I2C pins are configured as true open-drain I/O internally, (P-buffer and protection diode to VDD are not implemented)

    so is not possible to use them as output pins

    '', I don't know if I am right, is there any underlying risk to use I2C pins as output?

    Thanks and Regards

    jeffrey23
    Associate III
    May 17, 2011 1:08 PM UTC
    Posted on May 17, 2011 at 15:08

    Dennis,

    Do you mean that STM8S103F3 PB.4/PB.5 can be used

    as normal Open Drain pins ? Could you tell me how to configure their regisers ?

        // Init Port B

        /*

        [2]101

               7 6 5 4 3 2 1 0

               | | | | | | | |

               | | | |_________ I2C SCL (Output)    Open drain output

               | | |___________ I2C SDA (Output)    Open drain output

        DDR    0 0 1 1 0 0 0 0

        CR1    0 0 0 0 0 0 0 0

        CR2    0 0 0 0 0 0 0 0

        */

        GPIOB->DDR = 0x30;

        GPIOB->CR1 = 0x00;

        GPIOB->CR2 = 0x00;

    Are they  correct ? What did I miss else ?