Skip to main content
Associate II
June 27, 2023
Question

"STM8S103F3" is not working without "ST-V2 LINK" connection (NRST remains LOW)

"STM8S103F3" works "OK" and code is running while STV2 link (SWIM, RST, 3.3V, Ground) is connected with the application board and 3.3V supply is given to the application board from external power source.

But when I tried it to run without "ST-V2 LINK" connection, "STM8S103F3" does not work. What I observed that it's "NRST" pins remains "LOW" through out the time in this condition. I also tried to pull this pin to 3.3V with 47k, 10k but it remains "LOW".

    This topic has been closed for replies.