Associate
January 21, 2025
Question
STM8S103 Code Upload / Execution Issue
- January 21, 2025
- 4 replies
- 3851 views
Issue with STM8S103 Code Uploading on Identical PCB Boards
I have two identical PCB boards, both equipped with the STM8S103 microcontroller. One board functions perfectly, with code uploading and running as expected, while the other does not.
Observations
Voltage Measurements
- On the non-working board:
- NRST pin: 1.6V
- SWIM pin: 3.2V
- On the working board:
- NRST pin: 3.2V
- SWIM pin: Floating around 200mV
- On the non-working board:
Microcontroller Replacement
- Suspecting a defective STM8S103 on the non-working board, I desoldered it and placed it on a functioning development board (See the attachement).
- To my surprise, the board started working perfectly—code uploaded and executed without issues.
- I measured the voltage on the NRST and the SWIM pins. which were same as in the working board mentioned above.
- This indicates that the microcontroller on the non-working board is not faulty.
Setup
- Development Tools:
- SDUINO
- Arduino IDE
- ST LINK V2
I would greatly appreciate any insights or suggestions to identify the root cause of this issue
Thank you!