Skip to main content
HMoel.1
Associate II
August 20, 2020
Question

STM8S005K6 Bootloader no responding at data

Hi

I have a problem when I start writing the first page of the program.

I am running at 115200 8 data bit, 1 stop, no parity.

I am running in ECHO mode, meaning I return all bytes from the bootloader.

I have send the SYNC byte, at power up, and getting an ACK back ( which is being ECHO'ed back to bootloader)

Command is set (and its inverted ), and I am getting an ACK back (which is ECHO'ed back to bootloader)

Page is send (0x00008000) and the checksum.. The bootloader sends an ACK back (and I ECHO this back too).

Now when I send the page (N-1, [N bytes], checksum) I do not get anything.

I have tried sending more bytes (if the first byte was not interpreted correctly), changed baudrate, tried EVEN parity, etc..., but everything just gets me here..

I have tried sending an illegal command (inverted incorrect), and then I get a NAK as expected.

Can anyone point me in the correct direction?

    This topic has been closed for replies.

    2 replies

    HMoel.1
    HMoel.1Author
    Associate II
    August 25, 2020

    Further information

    If I change the address of the page to write to internal memory (0x00 or 0x80), I get the expected acknowledge back, but if the page is EEprom (0x4000) or Flash (0x8000) not response from STM8S is returned.

    HMoel.1
    HMoel.1Author
    Associate II
    August 27, 2020

    Update.

    I missed uploading the binary image for erase and write, as stated in UM560 paragraph 3.8.1

    Doing that prior to writing to flash, solved the isseus