Skip to main content
su shaowu
Visitor II
Feb 8, 2018 3:19 AM UTC
Question

STM8S001The UART Of Alternate function after remap,Unable to receive

Posted on February 08, 2018 at 04:19

Chip:STM8S001J3

The UART Of Alternate function after remap

RX is in PIN1?TX is in PIN5

The program has never been interrupted, RXNE has been 0.

What is the reason why you want to ask?

My configuration is as follows:

OPTION  BYTES?

                                AFR0?Alternate Active

                                 AFR1?Alternate Active

                                  AFR2?Alternate Active

Code?

            UART1_Init((uint32_t)9600, UART1_WORDLENGTH_8D,UART1_STOPBITS_1, UART1_PARITY_NO,

                   UART1_SYNCMODE_CLOCK_DISABLE, UART1_MODE_TXRX_ENABLE);

            UART1_ITConfig(UART1_IT_RXNE_OR, ENABLE);

             UART1_Cmd(ENABLE);

#the-program-has-never-been-interrupted #the-uart-of-alternate-function-after-remap #stm8s001j3
This topic has been closed for replies.

2 replies

Emilio P.G. Ficara
Associate
Apr 13, 2018 7:24 AM UTC
Posted on April 13, 2018 at 09:24

Look here:

https://community.st.com/0D50X00009XkX5uSAF

. The question is the same and the answer is: no answer. Not a valid solution has been presented. I made many attempts with interrupt, polling and various tricks, but nothing happened. Without the remapping, all works fine. It would be nice if some technician from ST would clarify the question. The STM8S001 component is good and cheap, but the 'swim' pin common to the UART TX is a strange / dangerous mapping arrangement.

Igor Cesko
ST Employee
Jun 29, 2018 8:15 AM UTC
Posted on June 29, 2018 at 10:15

 I confirm this mistake in documentation - it will be corrected in new datasheet (very soon). See the answer here

:

https://community.st.com/0D50X00009XkX5uSAF

 .