Skip to main content
bvn123
Associate II
May 28, 2020 9:38 PM UTC
Question

STM8S001J3 in halt mode: SWIM PROG error in IAR EWB. Is it possible to restore MCU programmability?

Hi,

Is it possible to restore STM8S001 for programming after set it to HALT mode?

I try to use halt mode for STM8S001 and STM8S003.

The programmer worked, when I used

__wait_for_interrupt();

but stopped after replacing this procedure to

__halt();

After set STM8S001 to halt mode I can't reprogram this MCU,

IAR EWB for STM8 shows the error:

'Failed to set configuration with MCU name STM8S001J3: SWIM PROG error [4]: Memory write error'

Now I try to test halt mode for STM8S003, but I added a cycle about 6-7s for SWIM PROG may start to work. As I see, SWIM PROG really works, when I start it during 6s after Power On, but doesn't start to work after this time.

Here is a program, which I loaded to STM8S001:

#include <intrinsics.h>
#include <iostm8s001j3.h>
 
#pragma vector = EXTI3_vector
__interrupt void PD_IRQhndl(void)
{
 PB_ODR_ODR4 = !PB_ODR_ODR4; // Toggle Port D, pin 3, STM8S001/cont.6
}
 
void main()
{
 __disable_interrupt();
 PB_ODR_ODR4 = 0; 
 PB_DDR_DDR4 = 1;
 PB_CR1_C14 = 1; 
 PB_CR2_C24 = 1; 
 
 for(unsigned long i=0;i<400000;i++){}; 
 //I placed this cycle to provide about 6s for SWIM PROG for STM8S003
 //There was not this cycle for STM8S001
 
 PB_ODR_ODR4 =1; //<LED & R=1k> may be connected between PB4 & +3V3 to indicate the end of 6s cycle
 
 PD_ODR_ODR6 = 1; 
 PD_DDR_DDR6 = 0;
 PD_CR1_C16 = 1; 
 PD_CR2_C26 = 1; 
 EXTI_CR1_PDIS = 2; 
 EXTI_CR2_TLIS = 0; 
 __enable_interrupt();
 
 while (1)
 {
 //__wait_for_interrupt();
 __halt();
 }
}

    This topic has been closed for replies.

    1 reply

    bvn123
    bvn123Author
    Associate II
    May 29, 2020 5:53 PM UTC

    I've restored the programmability of STM8S001J3, which have been going to HALT mode practically after Power On.