Skip to main content
whitehorsesoft
Associate III
May 15, 2026 8:25 AM UTC
Solved

STM8S TIM4 vs TIM2

Hello, I'm curious why TIM2 is correctly repeating in my code, whereas TIM4 with equivalent settings is not.

In this code, the TIM2 indicator (fired by the TIM2 interrupt) is blinking twice a second (clock set to LSI, meaning 128kHz). I would expect the TIM4 indicator (fired by the TIM4 interrupt) to do the same; but it is being triggered immediately and much faster: so fast that to the eye it appears as a constant on.

The reference manual RM0016 and datasheet DS7147 indicate that, given similar settings, both timers should be exhibiting similar behavior. What am I missing?

Here's the code:

; some typical setup hidden before this point
 ; PD3 is on, indicating LSI is clock source
 ld a, CLK_SWR
 cp a, #0xd2
 jrne 1$
 bset PD_ODR, #3

 ; timer setup
 sim
 ; F_Master Prescalar tim clk
 ; 128_000 Hz / 1024 = 125
 mov TIM2_PSCR, #0b1010 ; 2 ** 0b1010 = 1024 prescaler
 mov TIM2_ARRH, #0d0
 mov TIM2_ARRL, #0d125
 bset TIM2_IER, #0 ; UIE: Update interrupt enable
 bset TIM2_CR1, #0 ; CEN: Counter enable

 ; same as TIM2
 mov TIM4_PSCR, #0b1010
 mov TIM4_ARR, #0d125
 bset TIM4_IER, #0 ; UIE: Update interrupt enable
 bset TIM4_CR1, #0 ; CEN: Counter enable
 rim

 ; loop
 1$:
 wfi
 jp 1$

tim2_up_isr:
 bres TIM2_SR1, #0 ; UIF: Update interrupt flag
 ; blinks twice per second
 bcpl PC_ODR, #6
 iret

tim4_up_isr:
 bres TIM4_SR, #0 ; UIF: Update interrupt flag
 ; blinks continuously
 bcpl PC_ODR, #7
 iret

 

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 15, 2026 11:46 AM UTC

Yes, you missed one bit:

  • the prescaler of TIM2 (TIM2_PSCR, RM0016, 18.6.15, p. 244) can be set with PSC[3:0]
  • the prescaler of TIM4 (TIM4_PSCR, RM0016, 19.6.8, p. 259) can only be set with PSC[2:0]

As a result, for TIM4 with PSCR = (0b1010 AND 0b0111), this gives a prescaler of 4 instead of 1024, i.e. 256Hz instead of the required 1Hz.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

Peter BENSCH
ST Technical Moderator
May 15, 2026 8:32 AM UTC

TIM2 is a 16-bit timer, whereas TIM4 is only an 8-bit timer. Please take another look at your programme in light of this premise.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
whitehorsesoft
Associate III
May 15, 2026 8:59 AM UTC

> TIM2 is a 16-bit timer, whereas TIM4 is only an 8-bit timer.

Thank you for replying. I can understand when this would matter if I'm attempting to use values that wouldn't fit into an 8 bit timer. But in this case the ARR value for both timers is clearly able to fit into both 8 bits and 16 bits. Perhaps I'm overlooking something?

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 15, 2026 11:46 AM UTC

Yes, you missed one bit:

  • the prescaler of TIM2 (TIM2_PSCR, RM0016, 18.6.15, p. 244) can be set with PSC[3:0]
  • the prescaler of TIM4 (TIM4_PSCR, RM0016, 19.6.8, p. 259) can only be set with PSC[2:0]

As a result, for TIM4 with PSCR = (0b1010 AND 0b0111), this gives a prescaler of 4 instead of 1024, i.e. 256Hz instead of the required 1Hz.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.