Skip to main content
ib_gaus
Associate
Feb 3, 2010 6:02 PM UTC
Question

STM8S-Discovery USB communication

Posted on February 03, 2010 at 19:02

STM8S-Discovery USB communication

    This topic has been closed for replies.

    3 replies

    sramsauer9
    Visitor II
    May 17, 2011 1:07 PM UTC
    Posted on May 17, 2011 at 15:07

    Hello,

    maybe STVP programming toolkit can do the job.

    See documentation section 4.4.4 ''Reading the device''

    http://www.st.com/stonline/products/support/micro/files/um0151.exe

    http://www.st.com/stonline/books/pdf/docs/11472.pdf

    Regards,

    Stefan
    ib_gaus
    ib_gausAuthor
    Associate
    May 17, 2011 1:07 PM UTC
    Posted on May 17, 2011 at 15:07

    I know the embedded bootloader, but this is not suitable for my purpose.

    I would like to find an easy way to be able to communicate from a PC to the STM8 on the Discovery board using the already available USB connection. This would be possible, if I could send a USB command that sends a SWIM command for writing data into the RAM of the STM8 on-the-fly during normal program execution without stopping STM8. According to UM0470 ''STM8 SWIM communication protocol and debug module'', this should be possible using command WOTF (write on the fly).

    http://www.st.com/stonline/books/pdf/docs/14024.pdf

     

    But how to trigger such a WOTF over USB?

    Unfortunately there seems to be neither a tool nor a description of the used USB protocol. What a pity. This would offer much more possibilities for easy data exchange with a PC.

    patocheham2
    Visitor II
    May 17, 2011 1:07 PM UTC
    Posted on May 17, 2011 at 15:07

    Hello;

    The USB to SWIM protocol is proprietary, this is something ST doesn't want to disclosure.

    There are other ways to program the device . there is a bootloader embedded to be uses with the USART.