Skip to main content
RomainR.
ST Employee
Nov 30, 2010 9:31 AM UTC
Question

Stm8s Discovery project with stts75 sensor and µoled display

Posted on November 30, 2010 at 10:31

hello all

Please find attached file source code and resources on my recent personal project.

Stm8s-Discovery is interfaced with astts75 chip (digital I²C temprature sensor) and a graphic serialdisplay of the manufacturer μOled 96-SG1 4DSystems.

The accuracy of the temperature sensor can beselected by softwarefrom 0.5 ° C, 0.25 ° C, 0125 ° Cto 0.0625 ° C.

The scale measuring ranges from -55 ° C to +125 ° C.

The main program just displays the temperature on μOled with 0.5°C of accuracy.

I hope to improve this project very soon.

You can find the datasheet of stts75 here:

http://www.st.com/internet/analog/product/169jsp

4DSystems μOled display and serial here:

http://www.4dsystems.com.au/prod.php?id=77

Regards

Romain.

    This topic has been closed for replies.

    1 reply

    brazov22
    Associate III
    Dec 1, 2010 2:12 PM UTC
    Posted on December 01, 2010 at 15:12