Skip to main content
stock239955_st
Associate
Sep 15, 2010 8:16 PM UTC
Question

STM8S Discovery firmware - LCD display pinout

Posted on September 15, 2010 at 22:16

Hello

I'm trying to connect LCD display (WH1601A) to the demo board and use firmware SPI module and SPI_SimplexLCD example as base of my code.

But I can't see which PINs (ports) I should use to connect LCD display or where I can select MCU port. I found only ChipSelect and Backlight PINs configuration code (in

https://my.st.com//public/STe2ecommunities/mcu/Lists/STM8SDiscovery/mono__lcd_8h.html

). Could you please help me configure data port of say which port was used in sample program?

Thanks

Dmitry

null
    This topic has been closed for replies.

    4 replies

    mmaana
    Visitor II
    Sep 16, 2010 4:40 AM UTC
    Posted on September 16, 2010 at 06:40

    Hi, Dmitry!

    File mono_lcd.c is part firmwire for demoboard STM8/128-EVAL, LCD use on this board have SPI interfice, as connect this GLCD may see on schematic board (doc UM0842 - 

    http://www.st.com/mcu/familiesdocs-113.html

    ). 

    But why SPI? WH1601A not work in SPI mode.

    I use 4-bit mode for WH1602 on my STM8S-Discovery and no problems.

    Petr.

    Regards!

    stock239955_st
    Associate
    Sep 16, 2010 6:50 AM UTC
    Posted on September 16, 2010 at 08:50

    Petr,

    Thanks for you answer! I'm novice in MCU programming and firmware would help me with my experiments. I found couple libraries which work with LCD but was thinking firmware using is better way. I found LCD management example which uses SPI and planned modify them a little.

    But now I'm going to try with third-party libraries.

    Dmitry

    mmaana
    Visitor II
    Sep 16, 2010 7:38 AM UTC
    Posted on September 16, 2010 at 09:38

    Hi, Dmitry!

    If you new in world programming MCU, the fastest and simplest way (IMHO) to your case here

    http://atomsoft.wordpress.com/2010/03/08/lcd-on-stm8s-discovery/

     

    Regards!

    Petr

    stock239955_st
    Associate
    Sep 16, 2010 11:38 AM UTC
    Posted on September 16, 2010 at 13:38

    Petr,

    I'm already trying with this example;)

    Thanks