Skip to main content
Associate III
April 10, 2024
Question

STM8S bootloader Wireshark Dissector?

I am using the STM8S bootloader via a USB/FTDI.  I can use Wireshark/USBpcap and catch the exchanges and I have a somewhat happy "export packets, parse with Python" method of looking at the exchange.

But has anyone already written a proper Wireshark dissector for this?

    This topic has been closed for replies.

    2 replies

    Uwe Bonnes
    Chief
    April 10, 2024

    It seems, STM8 has no DFU bootloader. So I understand you that you have a serial to USB converter in between STM8 and PC and you want to spy on the USB side? Why dont you spy on the serial lines? Did you have a look at STM8 Flash loader demonstrator (UM0462,AN2606 and  AN3155))? Protocoll seem similar to STM32 serial bootloader. Maybe stm32flash can be modified? What are you trying to achieve anyways?

    Associate III
    April 10, 2024

    I have already implemented the bootloader for an stm8s but the uploading a new app failed.  By catching the exchange between the flasher and bootloader using Wireshark/USBpcap, exporting the frames and then writing a quick-n-dirty python script I was able to see that it is the "write" operation failing.

    Of course I could capture the data by getting more hardware and monitoring the serial lines instead of the USB traffic, and then writing a custom capture tool and dissector but it I'm going to go to that trouble I figured why not just use existing tools and write a Wireshark dissector directly since Wireshark/USBpcap can already monitor the flows for me.

    But of course if someone else has already written the Wireshark dissector, I would not need to even write a Wireshark dissector :-).