Skip to main content
gibba
Associate II
Dec 17, 2013 12:26 AM UTC
Question

STM8L152C6T6 - PWM output compare

Posted on December 17, 2013 at 01:26

Hi everyone,

I need to generate a square wave and I've written some code but it doesn't work as i want. Can anyone help me with my doubts please?

first of all: I'm not sure that the following registers are in hexadecimal.. any ideas?

second: I didn't undestand what are the complementary output states PRACTICALLY.

third: any advices on this code? 

Thanks a lot for every help,

Gilberto

uint16_t TIM1_Prescaler=4;

uint16_t TIM1_Period=320; 

uint8_t TIM1_RepetitionCounter = 0;

uint16_t TIM1_Pulse = 190;

CLK_PeripheralClockConfig(CLK_Peripheral_TIM1, ENABLE);

TIM1_DeInit();

TIM1_TimeBaseInit(TIM1_Prescaler,TIM1_CounterMode_Up,TIM1_Period,TIM1_RepetitionCounter);

TIM1_OC1Init( TIM1_OCMode_PWM1,

                  TIM1_OutputState_Enable,

                  TIM1_OutputNState_Disable,

TIM1_Pulse,

                  TIM1_OCPolarity_High,

                  TIM1_OCNPolarity_Low,

                  TIM1_OCIdleState_Set,

                  TIM1_OCNIdleState_Reset);

TIM1_OC1PreloadConfig(ENABLE);

TIM1_ARRPreloadConfig(ENABLE);

TIM1_Cmd(ENABLE);

#stm8l-stm8-pwm
    This topic has been closed for replies.

    1 reply

    chen
    Associate II
    Dec 17, 2013 9:51 AM UTC
    Posted on December 17, 2013 at 10:51

    Hi

    ''I'm not sure that the following registers are in hexadecimal.. any ideas?''

    In general, if you do not specify the number format the compiler will assume

    the number is in decimal.

    So

    ''

    uint16_t TIM1_Prescaler=4;

    uint16_t TIM1_Period=320; 

    uint8_t TIM1_RepetitionCounter = 0;

    uint16_t TIM1_Pulse = 190;''

    This code will set the registers to

    4

    320

    0

    190

    all in decimal.

    To specify the number in hexadecimal add '0x' in front of the number

    eg 0x0 = 0 decimal

    0xf = 15 decimal.

    Sorry, cannot help with the timer setup - I work on stm32 not stm8