Skip to main content
dhutchison1945
Associate III
Apr 26, 2011 8:13 AM UTC
Question

STM8L151K4 adc input impedance

Posted on April 26, 2011 at 10:13

STM8L151K4 adc input impedance

    This topic has been closed for replies.

    3 replies

    dhutchison1945
    Associate III
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Dear lowpowermcu,

    no,the rain(50kohm max) is the external resistor that you add in order to limitate the input current.

    I want to know the adc input pin impedance,but I think that I can see only the leakage current.

    b.r.

    spectre

    lowpowermcu
    Associate III
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Hi spectre,

    In the datasheet, I have found

    RAIN: External resistance on VAIN. It is equal to 50 KOhm.

    I think it the input impedance you are looking for.

    fggnrc2
    Associate III
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Hello Spectre!

    I agree with you: I found only the leakage current which is mainly due to the internal ESD protection diodes.

    You have also to take into account the current which the ADC draws in the sampling phase. This current depends on the input capacitance, whose value can be found in the datasheet too.

    However, leakage current is usually a few microamps, so you can estimate ADC input resistance as one MOhm.

    Regards,

    EtaPhi