Skip to main content
Esten.11
Associate
April 27, 2021
Question

stm8l151g4 DMA USART recieve only once

Hi.

i'm try using USART1 and recieve bytes with DMA from SBUS transmitter.

. But have strange problem - i'm recive only once and later DMA IRQ TC2 never occure. I'm try many variants - all not help me(((

Here my some code -

#define USART_DMA_CHANNEL_RX DMA1_Channel2
#define USART_DMA_CHANNEL_TX DMA1_Channel1
#define USART_DMA_FLAG_TCRX (uint16_t)DMA1_FLAG_TC2
#define USART_DMA_FLAG_TCTX (uint16_t)DMA1_FLAG_TC1
#define USART_DR_ADDRESS (uint16_t)0x5231 /* USART1 Data register Address */
#define USART_TX_BUF_ADDR (uint32_t)(&dma_pack)
 
uint8_t dma_pack[40];
 
static void USART_Config( void )
{
 CLK_PeripheralClockConfig( CLK_Peripheral_USART1, ENABLE );
 
 SYSCFG_REMAPPinConfig( REMAP_Pin_USART1TxRxPortA, ENABLE );
 
 GPIO_ExternalPullUpConfig( GPIOA, GPIO_Pin_3, ENABLE );
 GPIO_ExternalPullUpConfig( GPIOA, GPIO_Pin_2, ENABLE );
 
 USART_Init( USART1, ( uint32_t )100000, USART_WordLength_9b, USART_StopBits_2,
 USART_Parity_Even, ( USART_Mode_TypeDef )( USART_Mode_Rx ) );
 
 USART_Cmd( USART1, ENABLE);
}
 
static void DMA_Config( void )
{
 DMA_GlobalDeInit();
 
 DMA_DeInit( USART_DMA_CHANNEL_TX );
 DMA_DeInit( USART_DMA_CHANNEL_RX );
 
 CLK_PeripheralClockConfig( CLK_Peripheral_DMA1, ENABLE );
 
 DMA_Init( USART_DMA_CHANNEL_RX, USART_TX_BUF_ADDR, USART_DR_ADDRESS, 
 SBUS_PACKET_SIZE, DMA_DIR_PeripheralToMemory, DMA_Mode_Normal, 
 DMA_MemoryIncMode_Inc, DMA_Priority_Low, DMA_MemoryDataSize_Byte );
 
 DMA_ITConfig( USART_DMA_CHANNEL_RX, DMA_ITx_TC, ENABLE );
 DMA_Cmd( USART_DMA_CHANNEL_RX, ENABLE );
 USART_DMACmd( USART1, USART_DMAReq_RX, ENABLE );
 
 DMA_GlobalCmd( ENABLE );
 
}
 
 
INTERRUPT_HANDLER( DMA1_CHANNEL2_3_IRQHandler, 3 )
{
 if ( DMA_GetFlagStatus( DMA1_FLAG_TC2 ) != RESET )
 
 DMA_Cmd( DMA1_Channel2, DISABLE );
 DMA_SetCurrDataCounter( DMA1_Channel2, 25 );
 DMA_Cmd( DMA1_Channel2, ENABLE );
 DMA_ClearFlag( DMA1_FLAG_TC2 );
 
 }
}
 
main()
{
CLK_SYSCLKDivConfig( CLK_SYSCLKDiv_1 );
USART_Config();
DMA_Config();
while(1);
}

But IRQ dma2 fired only once and not later and program always stay in while loop.

There no problem in UART sender - uart-usb reciever working good and always getting SBUS packets..

Where maybe problem?

    This topic has been closed for replies.

    2 replies

    Esten.11
    Esten.11Author
    Associate
    April 27, 2021

    This is because USART overrun error - but why? Using circle dma not helping. Bug?

    WilkoL
    Senior
    April 28, 2021

    Are you sure you want to use 100 kbits/s, 9 bits data, even parity and 2 stopbits? It seems very unusual.

    115200 bps, 8 bits, no parity and 1 stopbit perhaps?