Skip to main content
Associate II
July 14, 2025
Solved

STM8L151G3 TIM4 not working

MCU: STM8L151G3U6
ISSUE: TIM4 interrupt doesnt seem working 
Connections:
                 1. LED on pin PB0
                 2. Push button/ switch on pin PC5

Scenario:
1. User press the push button

2. Toggles the LED

Observation:
Without using the TIM4 interrupt, the code works perfectly fine, when the TIM4 is used, the excutions reaches the first wait_50ms(); (red colour) and never go beyond this line, I would appreciate if any one would address the issue. BTW: I have used IRQHandler, 23  also but same result.

/===== Header files ======
#include "stm8l15x.h"

// Software timing counters
volatile uint16_t tick_1ms = 0;
volatile uint8_t flag_50ms = 0;
volatile uint8_t flag_100ms = 0;
volatile uint8_t flag_1min = 0;
volatile uint16_t soft_50ms = 0;
volatile uint16_t soft_100ms = 0;
volatile uint16_t soft_1min = 0;

//==== System Clock Configuration =====
void CLK_Config(void)
{
 CLK_DeInit(); // Reset the clock to its default setting
 CLK_HSICmd(ENABLE);// Enable the internal clock speec osscilator ( HSI = 16 MHz)
 while(CLK_GetFlagStatus(CLK_FLAG_HSIRDY) == RESET);// Wait until HSI is ready and stable
 CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_HSI);// Set HSI as a system clock source
 CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1); // Set system clock prescaler: devide by 1(full 16 MHz)
}

void TIM4_Config(void)
{
 TIM4_DeInit();
 TIM4_TimeBaseInit(TIM4_Prescaler_128, 125); // 16MHz / 128 = 125kHz; 125 -> 1ms
 TIM4_ClearFlag(TIM4_FLAG_Update);
 TIM4_ITConfig(TIM4_IT_Update, ENABLE);
 TIM4_Cmd(ENABLE);
}

INTERRUPT_HANDLER(TIM4_UPD_OVF_TRG_IRQHandler, 25)
{
 TIM4_ClearITPendingBit(TIM4_IT_Update);

 tick_1ms++;

 if (++soft_50ms >= 50) {
 soft_50ms = 0;
 flag_50ms = 1;
 }

 if (++soft_100ms >= 100) {
 soft_100ms = 0;
 flag_100ms = 1;
 }

 if (++soft_1min >= 60000) {
 soft_1min = 0;
 flag_1min = 1;
 }
//TIM4_ClearITPendingBit(TIM4_IT_Update);
}

// Utility: wait for 50ms debounce
void wait_50ms(void)
{
 flag_50ms = 0;
 while (!flag_50ms);
}

void wait_100ms(void)
{
 flag_100ms = 0;
 while (!flag_100ms);
}


//==== Main Function =====
int main()
{
 uint8_t system_on = 0; // 0 = off, 1 = on
 

 GPIO_Init(GPIOC, GPIO_Pin_5, GPIO_Mode_In_PU_No_IT); // Initialize Buttons Input
 GPIO_Init(GPIOB, GPIO_Pin_0, GPIO_Mode_Out_PP_Low_Fast); // Initialize LEDS

 CLK_Config(); // System clock
 TIM4_Config();
 enableInterrupts();



 while(1)
 {
 
 if(GPIO_ReadInputDataBit(GPIOC, GPIO_Pin_5) == RESET)
 {
 wait_50ms();
 if(system_on == 0)
 {
 // Turn on system
 system_on = 1;

 GPIO_SetBits(GPIOB, GPIO_Pin_0);

 // Blink twice
 GPIO_ToggleBits(GPIOB, GPIO_Pin_0);
 wait_100ms();
 GPIO_ToggleBits(GPIOB, GPIO_Pin_0);
 wait_100ms();
 }
 else
 {
 // Turn off system
 system_on = 0;
 GPIO_ResetBits(GPIOB, GPIO_Pin_0);
 }

 while(GPIO_ReadInputDataBit(GPIOC, GPIO_Pin_5) == RESET)
 wait_50ms();
 }
 }
}

Edited to apply source code formatting - please see How to insert source code for future reference.

    This topic has been closed for replies.
    RobK1
    RobK1Best answer
    Associate II
    July 14, 2025

    You don't seem to have the peripheral clock for the timer enabled:

    CLK_PeripheralClockConfig(CLK_Peripheral_TIM4, ENABLE);

    1 reply

    RobK1
    RobK1Best answer
    Associate II
    July 14, 2025

    You don't seem to have the peripheral clock for the timer enabled:

    CLK_PeripheralClockConfig(CLK_Peripheral_TIM4, ENABLE);