Skip to main content
Dmitry A
Visitor II
Oct 15, 2015 1:12 PM UTC
Question

STM8L101 clocking at < 2 MHz

Posted on October 15, 2015 at 15:12

Hello All, 

Is there any way to run STM8L101 at a frequency about 200 kHz to save some microAmps?

BR, Dmitry

#frequency #stm8l101
    This topic has been closed for replies.

    2 replies

    Ian Legg
    Visitor II
    Oct 19, 2015 8:04 AM UTC
    Posted on October 19, 2015 at 10:04

    Hi Dimitry,

    The L101 only looks to have the internal 16MHz RC clock, so an external crystal is not possible. However, you could adjust the CLK_CKDIVR to 64 for a 250KHz clock.

    Hope that helps.

    Ian

    toppot2009
    Associate II
    Oct 25, 2015 12:15 PM UTC
    Posted on October 25, 2015 at 13:15

    Добрый день, Дмитрий

    В stm8l101 �?огла�?но референ�? мануал не уда�?т�?�? уменьшить тактовую ча�?тоту ниже 2 МГц при и�?пользовании HSI (внутреннего RC генератора). Един�?твенна�? возможно�?ть уменьшени�? потреблени�? до микроампер �?то и�?пользовать режим Active-halt �?овме�?тно �? Auto-wakeup.