Skip to main content
Associate
September 30, 2024
Question

STM8L052R8 Watchdog Timer Issue

I have configured the watchdog for the maximum duration possible, i.e, 1.7 sec. 

void watchdog_init(void)
{
CLK_ICKCR |= CLK_ICKR_LSION;
IWDG_KR = 0x55; 
IWDG_PR = 6; 
IWDG_RLR = 0xFF;
IWDG_KR = 0xCC; 
}

But it seems to be resetting in around 26 - 28 ms. I have also checked this timing with an oscilloscope by toggling a led. 

watchdog_init();
do {
LED5_TOGGLE();
printf("Test!\n");
delay(516);
} while(1);
  
What do you think is the cause for this issue? How is it possible to fix this? 
    This topic has been closed for replies.

    1 reply

    AA1
    Senior III
    September 30, 2024

    As explained in RM, the first step must be enable the watchdog. As is, the watchdog is using the reset values.

    Use this code:

    void watchdog_init(void)
    {
    CLK_ICKCR |= CLK_ICKR_LSION;
    IWDG_KR = 0xCC; // enable
    IWDG_KR = 0x55; // write access
    IWDG_PR = 6;
    IWDG_RLR = 0xFF;
    IWDG_KR = 0xAA; // refresh
    }

    ,