Skip to main content
KKURT
Associate
Mar 15, 2019 11:21 AM UTC
Question

STM8L051

Hi, I am not sleeping this microcontroller. I search example code but I couldnt find it please help me. Thanks.

    This topic has been closed for replies.

    5 replies

    Sisto Zànier
    Senior
    Mar 15, 2019 3:39 PM UTC

    /*

    hi, I don't know what you mean, but to sleep the micro you can use Halt mode.

    This can be a possible solution:

    To enter HALT mode:

    */

    void HALT_INIT (void)

    {

      ADC_Cmd (ADC1, DISABLE);

      PWR_PVDCmd (DISABLE);

      / * Switch to LSI as system clock source * /

      / * system clock prescaler: 1 * /

      CLK_SYSCLKDivConfig (CLK_SYSCLKDiv_1);

      CLK_SYSCLKSourceConfig (CLK_SYSCLKSource_LSI);

      CLK_SYSCLKSourceSwitchCmd (ENABLE);

      while (CLK_GetFlagStatus (CLK_FLAG_LSIRDY) == 0);

      CLK_HSICmd (DISABLE);

      CLK_HSEConfig (CLK_HSE_OFF);

    CLK_HaltConfig (CLK_Halt_SlowWakeup, ENABLE);

      / * Set STM8 in low power * /

      PWR_UltraLowPowerCmd (ENABLE);

    }

    .....

    void main ()

    {

    INIT_MICRO_PARAMS (); // Depending from your hardware and GPIO configurations

    INIT_ADC_PARAMS ();

    #if (_USE_RTC)

    INIT_RTC (); 

    CLK_HaltConfig (CLK_Halt_SlowWakeup, ENABLE);

    #endif

    enableInterrupts ();

    while (1)

    {

     // insert here Your code executed in run mode

     HALT_INIT (); // Switch oscillator from HSI to LSI

     halt (); // Enter "Active-Halt" mode for halt consumption of about 5uA. 

     // in debug mode with ST-LINK/V2, use wfe() instead of halt()

    }

    }

    /*

    To exit from HALT mode you can use a micro Reset, or a periodic interrupt from RTC properly configured to generate it, or a GPIO interrupt (see reference manual RM0031)

    I hope thi suggestion can help You

    */

    KKURT
    KKURTAuthor
    Associate
    Mar 18, 2019 8:37 AM UTC
    [cid:02918b84-722e-4abc-8254-4b0cc93952d5][cid:2443039c-cf3d-4f5d-8eaa-5f61e327cfc9]

    Thank you for your interest. Halt mode current normally 5uA but me 92uA this too much. I think I'm doing something wrong. Don't understand. Can you help me this topic?
    Max
    ST Employee
    Mar 18, 2019 3:43 PM UTC

    Hello, have you looked at AN3147?

    KKURT
    KKURTAuthor
    Associate
    Mar 26, 2019 7:07 AM UTC
    I tried but not again. What else can I do?
    Cristian Gyorgy
    Associate II
    Mar 31, 2019 1:11 PM UTC

    How do you measure the 92 µA? Does you MCU not wake up and do things between sleeping?

    Post your schematics. Active pull-ups, ports, or other consumers?

    You should post more info if you want help.