Skip to main content
jisoon
Associate
August 23, 2011
Question

STM8L power (current) consumption problem

Posted on August 23, 2011 at 06:42

 I'm developing some applications with STM8L152R8 and STM8L152M8 MCU now, and both applications are battery-used product. The problem is that, I cannot make the MCU consume micro-ampere order current.

 I used every methods described in the reference guide manual, including low power run mode, active halt mode, and halt mode but our current indicator displayed mA order current consumption, from 1mA to 5mA. Of course I have stoped HSI, LSI, all timers and disabled all interrupts. GPIOs are also retested as push-pull low-slow output mode. I was confused, thus I decided to take out the STM8L discovery board and verify with that evaluation board.

 First, I just delivered power into the discovery board with USB cable. Through toggling the power mode, the LCD of discovery board have shown fine current consumption. About 1mA in run mode, and about 7uA in low-power mode, and below 1uA in halt mode ... it seemed fine.

 However, the result changed with my verification method changing. I switched the IDD jumper to 'OFF' mode, and started verification again. With IDD jumper switch off, the current-measuring circuit should be powerless and the MCU will solely consume the power, I expected so. I connected the precise current measuring multimeter (Agilent 34401A) serially in power supply line (3.3V), and started current consumption measuremnt by ourselves. And the multimeter have shown 30mA of current consumption. Unbelievable, but that's what I've seen. Regardless of MCU power mode, the current consumption was 30mA.

 This is my current situation. Now I cannot be certain of our current consumption method neither the firmware code we've written for MCU low power mode. I want to run our device in active-halt mode with RTC, and the power consumption matter is very important. 

 Little help here, please?

#stm8s-discovery-power-consumption #low-power #stm8l #stm8l-low-power-halt #high-current #high-current
This topic has been closed for replies.

13 replies

komarek.milan
ST Employee
August 23, 2011
Posted on August 23, 2011 at 14:06

Hello,

Where did you connect the amp meter exactly? It should be connected between JP1 header pin 1 and 2 of the STM32L Discovery otherwise you are measuring something else than the microcontroller current consumption.

jisoon
jisoonAuthor
Associate
August 24, 2011

Posted on August 24, 2011 at 02:21

Thank you eM Ko, You pointed out well ... I guess I measured current from wrong pins. I measured current between +3V3 and GND pin, which are supplying power into ST-LINK as well. Measuring between JP1 pin 1 and 2, the measured current consumption was fine.

Now my remaining problem is about setting my own target application MCU into low power consumption mode. The code below is my source code which intended to make MCU go into active halt mode. Anybody please point out what's wrong here?

////////////////////////////////////////////////////////
LCD_Cmd(DISABLE);
CLK_PeripheralClockConfig(CLK_Peripheral_LCD, DISABLE);
CLK_PeripheralClockConfig(CLK_Peripheral_ADC1, DISABLE);
CLK_PeripheralClockConfig(CLK_Peripheral_USART1, DISABLE);
CLK_PeripheralClockConfig(CLK_Peripheral_USART2, DISABLE);
CLK_PeripheralClockConfig(CLK_Peripheral_TIM1, DISABLE);
CLK_PeripheralClockConfig(CLK_Peripheral_TIM2, DISABLE);
CLK_PeripheralClockConfig(CLK_Peripheral_TIM3, DISABLE);
CLK_PeripheralClockConfig(CLK_Peripheral_TIM4, DISABLE);
CLK_PeripheralClockConfig(CLK_Peripheral_TIM5, DISABLE);
TIM1_Cmd(DISABLE);
TIM2_Cmd(DISABLE);
TIM3_Cmd(DISABLE);
TIM4_Cmd(DISABLE);
TIM5_Cmd(DISABLE);
ITC_DeInit();
CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1);
CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_LSI);
CLK_SYSCLKSourceSwitchCmd(ENABLE);
while (((CLK->SWCR)& 0x01)==0x01);
CLK_HSICmd(DISABLE);
CLK->ICKCR |= 0x10; CLK->ICKCR &= ~0x20; CLK->ICKCR &= ~0x40; CLK->ICKCR |= 0x04; CLK->ICKCR &= ~0x01;
CLK_MainRegulatorCmd(DISABLE);
PWR_UltraLowPowerCmd(ENABLE);
GPIO_Init(GPIOA, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Slow);
GPIO_Init(GPIOB, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Slow);
GPIO_Init(GPIOC, GPIO_Pin_2|GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Slow);
GPIO_Init(GPIOC, GPIO_Pin_0|GPIO_Pin_1, GPIO_Mode_Out_OD_Low_Slow);
GPIO_Init(GPIOD, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Slow);
GPIO_Init(GPIOE, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Slow);
GPIO_Init(GPIOF, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Slow);
GPIO_Init(GPIOG, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Slow);
GPIO_Init(GPIOI, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3, GPIO_Mode_Out_PP_Low_Slow);
sim();
halt();
henry.dick
Associate II
June 11, 2018
Posted on June 11, 2018 at 12:11

'

I measured current between +3V3 and GND pin,'

you couldn't have possibly done that. because if you did, you would have blown up either the power supply or the meter.

what you described is weird (out of this worldly weird), and more likely a measurement problem. If I were, you, I would take out a schematic and show exactly how and where you measured the current and go from there.

jfelix
Associate II
September 28, 2011
Posted on September 28, 2011 at 10:36

Hello lim.jisoon,

I have the exact same problem, I wrote a similar function as yours to enter active halt mode but current consumption is still nearly the same. Did you succeded to get very low current consumption?

Viktor POHORELY
ST Employee
September 29, 2011
Posted on September 29, 2011 at 16:48

Try this one... it's for 152C6, so some adjustments to your sales type could be needed.

________________

Attachments :

Active_HALT.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzNk&d=%2Fa%2F0X0000000bKs%2Ffo7zkjPo3exxd75hJi86lUD8pwql0WsZDs0cljZUelk&asPdf=false
Ali Abdal-Kadhim
Associate
June 11, 2018
Posted on June 11, 2018 at 09:34

thank you very much for the example code attached, it is really helpful. but, I am new to this brand of low power MCUs and currently I have a research on the low power MCUs. I faced a problem on how to make the stm8l

152C6 

MCU wake up again from the halt period of let's say 10 seconds. I.e. the mentioned MCU will halt for 10 seconds and then wake up to flash the LEDs and then go to halt again.  

Thank you pretty much. 

jisoon
jisoonAuthor
Associate
October 5, 2011
Posted on October 05, 2011 at 03:22

 Hello felix,

 My problem turned out to be voltage supply dependent one. 

 The current consumption of STM8L is very sensitive to the level of voltage supply. The specification of STM8L current consumption is all measured in 3V Vcc. If you increase the Vcc to 3.3V, the current consumption increases dramatically. 

 Try to add a 3.0V LDO in front of your MCU voltage supply line and measure the current consumption of your STM8L MCU. This is how I solved this problem. 

 Good luck!

elil
Associate III
October 11, 2011
Posted on October 11, 2011 at 18:31

Very strange, as IMHO, STM8L should not be sensitive to  Vcc since it has internal voltage regulator.

kkarasti
Associate II
February 3, 2012

Posted on February 03, 2012 at 16:49

Here's what I'm doing for the STM8L151 and it drops current to 0.5uA. This is full halt, but if you want to keep RTC active, just comment out those lines. One thing, you have to clear the wakeup INT before halt. Here, I'm using EXTI pin7 for wakeup.

Halt_Init();
EXTI_ClearITPendingBit(EXTI_IT_Pin7);
halt();

void Halt_Init(void)
{
 TIM1_Cmd(DISABLE);
 TIM2_CtrlPWMOutputs(DISABLE);
 TIM2_Cmd(DISABLE);
 TIM3_Cmd(DISABLE);
 TIM4_Cmd(DISABLE);
 ADC_Cmd(ADC1, DISABLE);
 PWR_PVDCmd(DISABLE);
 /* Switch to LSI as system clock source */
 /* system clock prescaler: 1*/
 CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1);
 CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_LSI);
 CLK_SYSCLKSourceSwitchCmd(ENABLE);
 while (CLK_GetFlagStatus(CLK_FLAG_LSIRDY) == 0);
 CLK_HSICmd(DISABLE);
 CLK_HSEConfig(CLK_HSE_OFF);
 /* Set STM8 in low power */
 PWR_UltraLowPowerCmd(ENABLE);

 /* Set GPIO in low power*/
 GPIO_LowPower_Config();

 /* Stop RTC Source clock */
 CLK_RTCClockConfig(CLK_RTCCLKSource_Off, CLK_RTCCLKDiv_1);

 /* Stop clock RTC and LCD */
 CLK_PeripheralClockConfig(CLK_Peripheral_RTC, DISABLE);
 CLK_PeripheralClockConfig(CLK_Peripheral_LCD, DISABLE);
}

void GPIO_LowPower_Config(void)
{
 /* Configure unused pins as output push-pull 0 to enter low power */
 /* Port A */
 GPIO_Init(GPIOA, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Slow);
 /* Port B not AIN */
 GPIO_Init(GPIOB, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Slow);
 /* Port B LEDs, so they don't flash at power on */
 GPIO_Init(GPIOB, GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5, GPIO_Mode_Out_PP_High_Slow);
 /* Port C not wakeup pin!! */
 GPIO_Init(GPIOC, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6, GPIO_Mode_Out_PP_Low_Slow);
 /* Port D */
 GPIO_Init(GPIOD, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Slow);
 /* Port E */
 GPIO_Init(GPIOE, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Slow);
 /* Port F */
 GPIO_Init(GPIOF, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Slow);
}
Associate
October 4, 2024

Hi, this is very helpful for my project, but with same code I am able to achieve only 0.8mA,

Please suggest, how to achieve 0.5uA as you suggested,

I am using STM8L151K4T6 IC, and connection multimeter (black and white pins) in parallel with Vcc to check current.

Like: multimeter red pin -> IC vcc and black pin -> stlink vcc

Tesla DeLorean
Guru
October 4, 2024

Understand this post is from 12 years ago, forum respondent unlikely to be checking thread, or alerted..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ivgenikucherov
Visitor II
December 11, 2013
Posted on December 11, 2013 at 13:48

Hi,

I am using stm8L051F3 micro controller.

In my system, 3.7V voltage is implied on VDD.

What is the minimal current consumption that I should measure in halt mode ?

According to datasheet, the typical is 350nA while maximum is 2microA on 1.8V to 3.6V voltage.

Thanks,

Ivgeni.