Skip to main content
richardaddy9
Associate II
Oct 26, 2016 9:18 AM UTC
Question

STM8L LCD Register

Posted on October 26, 2016 at 11:18

Hi, I'm using the STM8L052R8 for temperature measurement, so using an ADC channel, and then displaying the temperature on the LCD.

It would be really handy to be able to clear the LCD Ram memory instead of writing to every LCD Ram Register used. Is there a generic command that will do this for me, I can't see it anywhere.

Thanks in advance. 

    This topic has been closed for replies.

    1 reply

    Simon V.
    ST Employee
    Mar 6, 2017 10:54 AM UTC
    Posted on March 06, 2017 at 11:54

    Hi Addy,

    I checked the reference manual and there is no specific control bit to only clear the LCD_RAM content.

    Regards,

    Simon

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.