Skip to main content
Stm32User
Associate III
Apr 22, 2010 4:37 PM UTC
Question

STM8L Internal temperature Sensor

Posted on April 22, 2010 at 18:37

STM8L Internal temperature Sensor

#stm8l-temperature-sensor
    This topic has been closed for replies.

    3 replies

    will2
    Associate II
    May 17, 2011 1:08 PM UTC
    Posted on May 17, 2011 at 15:08

    That's a 12-bit A/D, right?  Which would make your A/D counts range 0 - 4095.  Wouldn't you expect to see maximum counts when you apply your Vref+ to the A/D?  The A/D values that you got back don't seem correct.

    Stm32User
    Stm32UserAuthor
    Associate III
    May 17, 2011 1:08 PM UTC
    Posted on May 17, 2011 at 15:08

    The ADC uses the VREF input as its reference in my case AVDD (+3V3).

    The device has an internal bandgap which can be connected to the input for scaling measurements. This is 1.23v nom so no I would not expect fullscale.

    I have discovered two things :-

    1) You need to wait 10uS after powering up the internal VRef before it is stable.  This delay gives me sensible readings.

    2) The datasheet has a typographical error.  The temperature sensor produces 1.62mV / Deg K not 1.62mV/DegC.  When calculating the temperature you need to subtract 273.15 !

    FordFairlane
    Associate III
    May 28, 2012 12:08 PM UTC
    Posted on May 28, 2012 at 14:08

    Hello

    I have searched for any application note to calculate microcontroller temperature but I have not found any information.

    Does anybody have a function to get the microcontroller temperature?, in that case could anybody share the source code?.

    Thank you un advance.

    Regards