Skip to main content
Artur L
Visitor II
May 14, 2017 7:52 PM UTC
Question

STM8L DISCOVERY ADC

Posted on May 14, 2017 at 21:52

Hello,

I want to create program that:

1. Measure time

2. Start one conversion of ADC

3. After conversion show it on LCD (it's optional, but it would be great if it works)

The 2nd point is problematic. I want to realize all on interrupts and my program doesn't jump into adc int handling.

Here is a ADC configuration:

void ADC_Periph_Init(void)

{

  CLK->PCKENR2|=0x01; //adc clock en

  ADC1->CR1|=0x01;  //adc ADON

  ADC1->SQR[0]|=0x81;  //select channel 24, DMA disable for single conversion

  GPIOF->DDR&=0xFE;

  GPIOF->CR1&=0xFE;

  GPIOF->CR2&=0xFE;  //gpio for adc configutation for PF0

  ADC1->CR1|=0x68;   //resolution, single conversion, enable interrupt end of conversion

  ADC1->CR2&=0x78; //sample time, PRESC=0

  ADC1->CR3=0x1F;  //sample time

  ADC1->CR1&=0xFE;

}

Here is TIM4 int

INTERRUPT_HANDLER(TIM4_UPD_OVF_TRG_IRQHandler, 25)

{

  TIM4->SR1&=0xFE; //clear flag from ovf

  if(((GPIOC->ODR&0x80)>>7)==0x01){

  GPIOC->ODR&=0x7F;

  }

  else{

  GPIOC->ODR|=0x80;  

  }

  if((GPIOA->IDR&0x08)==0x08)licznik2++;

  else licznik2=0;

  if ((licznik2==10)&&(~ADC_start_conv)){

  ADC1->CR1|=0x01;

  ADC_start_conv=TRUE;

  for(i=0;i>16000;i++)

  ADC1->CR1|=0x02;

  }

 

  TIM4->CNTR=0xFF-488;

return;

}

generally ADC->CR1|=0x01 is done when switch is on for a period of time.

I use IAR.

Where is the fault and how it should look properly?
    This topic has been closed for replies.