Skip to main content
JAn.1610
Associate II
November 14, 2019
Question

STM8001J3 - Cannot communicate with the device!

I used ST Visual Programmer to check if soldering's been completed well.

I didn't open any files but just clicked the programming tab (the red arrow one) but the message that it cannot communicate with the device popped up. It still didn't work when I opened '3op16icp.s19' and then programmed.

I had to use I2C, USART, and SWIM so on my PCB I connected USART_TX and SWIM on the same 8 pin, because I found out that if I give time delay before converting 8 pin into USART_TX I can still access it to SWIM pin beforehand.

And I left reset pin unconnected. I worried that if unconnected reset pin might cause problem so I tried it to connect whether ground or VCC, but it didn't work.

Can you tell me what the problem is with my chip?

Thanks

    This topic has been closed for replies.