Skip to main content
Kmax18
Senior II
December 28, 2022
Question

STM8 UART1 in half-duplex single-wire mode, switching between RX and TX

I am using a NUCLEO-S8208RB to develop UART1 communication in half-duplex, single-wire mode. The device receives messages (packets of bytes) using the UART1_IT_RXNE_OR interrupt. The next step would be to transmit a byte packet in response, without an interrupt. That does not work. I suspect the UART1_TX configuration is wrong.

* IDE: STVD with COSMIC compiler and STVP.

* STM8 Standard Peripheral Library.

UART1 configuration code (this works):

UART1_DeInit();
UART1_Init((uint32_t)UART1_BAUDRATE, UART1_WORDLENGTH, UART1_STOPBITS, UART1_PARITY, UART1_SYNCMODE, UART1_MODE_TXRX_ENABLE);
UART1_ITConfig(UART1_IT_RXNE_OR, ENABLE);
UART1_HalfDuplexCmd(ENABLE);
enableInterrupts();

The UART1_RX interrupt call function uses this code snippets:

void UART1_RX_Handler_Callback()
{
 uart1RxData_u8 = UART1_ReceiveData8();
 ...
 UART1_ITConfig(UART1_IT_RXNE_OR, DISABLE);
}

The following code for UART1_TX does not work. It 'hangs', likely due to wrong UART1 register settings. Please comment. Thank you!

void UART1_TransmitPacket8()
{
 uint8_t nBytesToSend = (uint8_t) PACKET_MAX_LEN;
 TxCounter1 = (uint8_t) 0;
 while (nBytesToSend > 0)
 { 
 while (UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET)
 { } 
 UART1_SendData8(uart1_TxBuffer_u8[TxCounter1]);
 nBytesToSend--;
 TxCounter1++; 
 }
 
 while (UART1_GetFlagStatus(UART1_FLAG_TC) == RESET)
 { }
}

    This topic has been closed for replies.

    2 replies

    AA1
    Senior III
    December 28, 2022

    UART1_SYNCMODE?

    Mode should be asynchronous.

    Kmax18
    Kmax18Author
    Senior II
    December 28, 2022
    Yes, asynchronous mode is on. Thanks you.