Skip to main content
pok-on
Associate II
Oct 16, 2013 8:36 AM UTC
Question

stm8_uart1.c error

Posted on October 16, 2013 at 10:36

Hello,

I am not sure if this is a proper place for reporting errors. If not so, please tell me, where to report it.

The error is in stm8_uart1.c module of STM8S_StdPeriph_Lib_V2.1.0.

According to description of UART1_ITConfig one of the parameters can have value UART1_IT_RXNE or UART1_OR. When using one of these, the assert_failed function will be called as macro IS_UART1_CONFIG_IT_OK(UART1_IT) treat them as invalid parameters. Using parameter UART1_IT_RXNE_OR works well with the same effect, but at least the description of UART1_ITConfig should be corrected to safe developers time ;-).

#uart1_itconfig-stm8s_stdperiph
This topic has been closed for replies.

1 reply

Dmitry Key
Associate
Feb 25, 2018 8:56 AM UTC
Posted on February 25, 2018 at 09:56

Same here. Had to replace function call with simple

UART1->CR2 |= (uint8_t)UART1_FLAG_RXNE;