Associate III
Oct 29, 2012 6:25 AM UTC
Question
stm8 uart1
- 3 replies
- 1889 views
Posted on October 29, 2012 at 07:25
hello,
please can someone one help me with a uart problem on the stm8s i use a crystal of 14.7456 Mhz , also i do the change of the clock system, see the atached program. the uart1 is initialised as, pa4 and pa5, also i use a second computer with the DOCKLIGHT program to analyze the communication. the uart is set for 9600 baud, 1 stop , 7 data even parity also the docklight program is set for that . if i send one character from the stm8s to the other computer i see that character correct. even with different characters no if i send a character from the docklight program on the other computeri also see that character correct in the stm8s data ram but if i will send a string of characters ,for example 81 82 83 84 85 from the docklight program,i receive in the stm8s data ram 81 82 03 84 05 i have tryed with other characters, and it seems then the 7 bit is always set to 1, some characters are correct please , is there any idea what i do wrong in the program see atached assembly program file many thanks marc debruyne